Enable RGB LED's and push buttons on 8MIC-RPI-MX8 board.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable RGB LED's and push buttons on 8MIC-RPI-MX8 board.

Enable RGB LED's and push buttons on 8MIC-RPI-MX8 board.

Useful information about push buttons.

 

Physical level.

 

 

JulioMeza_2-1642521492586.png

 

     When there is a change of voltage level on P0-P7 pins, PCA9555PW will generate interrupt on INT pin. The driver (running on SoC) can read the status of P0-P7 pins via I2C (SCL/SDA pins) and generate separate interrupts for each of P0-P7 pins. This is why this driver acts as interrupt controller.

Consider next configuration:

JulioMeza_3-1642521543516.png

 

     One push button changes level on P4 pin, tempting PCA9555PW to generate interrupt. Interrupt from PCA9555PW is connected to GPIO5 IP-core (inside of SoC), and it uses line #9 of that GPIO5 module to notify CPU about interrupt. So we can say that PCA9555PW is cascaded to GPIO5 controller. GPIO5 also acts as interrupt controller, and it's cascaded to GIC interrupt controller.

 

Device tree properties.

 

The meaning of properties is as follows:

  • interrupt-controller property defines that device generates interrupts; it will be needed further to use this node as interrupt-parent in each push button node.

  • #interrupt-cells defines format of interrupts property; in our case it's 2: 1 cell for line number and 1 cell for interrupt type

  • interrupt-parent and interrupts properties are describing interrupt line connection

 

Interrupt handling.

 

  • CPU now is in interrupt context in GIC interrupt handler. From gic_handle_irq() it calls handle_domain_irq(), which in turn calls generic_handle_irq(). See Documentation/gpio/driver.txt for details. Now we are in SoC's GPIO controller IRQ handler.

  • SoC's GPIO driver also calls generic_handle_irq() to run handler, which is set for each particular pin. See for example how it's done in omap_gpio_irq_handler(). Now we are in PCA9555PW IRQ handler.

  • PCA9555PW IRQ handler calls handle_nested_irq().

  • Finally, gpio_keys_gpio_isr() is called.

     The following steps allow you to enable rgb led's and push buttons on 8MIC-RPI-MX8 board with i.MX 8M Mini Applications Processor Evaluation Kit (EVKB). You have to use a led driver and change the device tree.

On the Host.

Cloning the Linux kernel repository.

 

Clone the i.MX Linux Kernel repo to the home directory.

cd ~
git clone https://source.codeaurora.org/external/imx/linux-imx

This guide will use the following commit which corresponds to Kernel 5.10.35-2.0.

cd linux-imx/
git checkout -b RGB ef3f2cfc6010

Patching the device tree.

 

Download the "0001-Enable-RGB-LED-s-and-push-buttons-on-8MIC-RPI-MX8-bo.patch" file attached to this post and copy it into linux-imx directory, then apply the patch.

cp 0001-Enable-RGB-LED-s-and-push-buttons-on-8MIC-RPI-MX8-bo.patch ~/linux-imx/
cd ~/linux-imx/
patch < 0001-Enable-RGB-LED-s-and-push-buttons-on-8MIC-RPI-MX8-bo.patch

When prompted, select the file to patch:

File to patch: arch/arm64/boot/dts/freescale/imx8mm-evk-8mic-revE.dts patching file arch/arm64/boot/dts/freescale/imx8mm-evk-8mic-revE.dts

Then setup your toolchain, for example:

source /opt/fsl-imx-wayland/5.10-hardknott/environment-setup-cortexa53-crypto-poky-linux

Generate config file.

make imx_v8_defconfig

Compile the device tree.

make freescale/imx8mm-evk-8mic-revE.dtb

Copy the .dtb file to the EVK, for example with scp:

scp imx8mm-evk-8mic-revE.dtb root@<EVK_IP>:/home/root

Alternatively, you may copy the .dtb file directly to the FAT32 partition where the Kernel and Device Tree files are located.

Compiling the Led driver.

 

Obtain the leds-pca995x.h file in the next site:

https://github.com/TechNexion/linux-tn-imx/blob/tn-imx_5.4.70_2.3.0-stable/include/linux/platform_da... 

Copy it into the next path:

cp leds-pca995x.h ~/linux-imx/include/linux

Create a new directory.

mkdir ~/linux-imx/PCA9955

Create a makefile.

cd ~/linux-imx/PCA9955
vim Makefile

 

KERNEL_ROOT?=~/linux-imx

obj-m += leds-pca995x.o

all: make -C $(KERNEL_ROOT) M=$(PWD) modules

clean: make -C $(KERNEL_ROOT) M=$(PWD) clean

 

Press the key "Esc" and then:

:wq

Obtain the leds-pca995x.c file in the next site:

https://github.com/TechNexion/linux-tn-imx/blob/tn-imx_5.4.70_2.3.0-stable/drivers/leds/leds-pca995x...

Copy it into the next path:

cp leds-pca995x.c ~/linux-imx/PCA9955

Obtain 0001-PCA9955BTW.patch file and copy it into the next path:

cp 0001-PCA9955BTW.patch ~/linux-imx/PCA9955

Apply the patch.

patch < 0001-PCA9955BTW.patch

Then setup your toolchain, for example:

source /opt/fsl-imx-wayland/5.10-hardknott/environment-setup-cortexa53-crypto-poky-linux

Generate .ko file.

cd ~/linux-imx/PCA9955
make all

Copy the .ko file to the EVK, for example with scp:

scp leds-pca995x.ko root@192.168.100.105:/home/root

NOTE: The linux version of .ko file must be the same as EVK.

On the EVK.

Switching the device tree.

 

To copy the updated device tree to the corresponding partition, first create a directory.

mkdir Partition_1

Mount the partition one.

mount /dev/mmcblk1p1 Partition_1/

Copy or move the device tree into partition one.

cp imx8mm-evk-8mic-revE.dtb Partition_1/

Reboot the board.

reboot

Stop on u-boot and modify the .dtb file to use the device tree for 8mic board.

u-boot=> editenv fdtfile 
edit: imx8mm-evk-8mic-revE.dtb 
u-boot=> saveenv 
Saving Environment to MMC... Writing to MMC(1)... OK 
u-boot=> boot

Installing a led driver.

 

Execute the following command to load the led driver into the kernel.

insmod leds-pca995x.ko

And you will see something like:

[ 249.359103] leds_pca995x: loading out-of-tree module taints kernel. 
[ 249.366864] ALL 
[ 249.368740] ALL 0 
[ 249.370667] ALL 1 
[ 249.372609] ALL 2 
[ 249.374536] ALL 2 
[ 249.376475] ALL 2 
[ 249.378401] ALL 2 
[ 249.380338] ALL 2 
[ 249.382264] ALL 2 
[ 249.384202] ALL 2 
[ 249.386127] ALL 2 
[ 249.388063] ALL 2 
[ 249.389989] ALL 2 
[ 249.391913] ALL 2 
[ 249.393847] ALL 2 
[ 249.395774] ALL 2 
[ 249.397709] ALL 2 
[ 249.399635] ALL 2 
[ 249.401568] ALL 2 
[ 249.403496] ALL 3

Turning on a Led.

 

If you changed the device tree, you can turn on a led with the following command:

echo 250 > /sys/class/leds/pca995x\:blue0/brightness

To turn off a led:

echo 0 > /sys/class/leds/pca995x\:blue0/brightness

The red, blue and green leds can be turned on at different intensities provided.

Testing the push buttons.

 

If you changed the device tree, you can test the push buttons with the following command:

evtest

Select the correct number:

No device specified, trying to scan all of /dev/input/event* 
Available devices: 
/dev/input/event0: 30370000.snvs:snvs-powerkey 
/dev/input/event1: sw_keys 
/dev/input/event2: gpio_ir_recv 
Select the device event number [0-2]: 1

And you will see:

Input driver version is 1.0.1 
Input device ID: bus 0x19 vendor 0x1 product 0x1 version 0x100 
Input device name: "sw_keys" 
Supported events: 
  Event type 0 (EV_SYN) 
  Event type 1 (EV_KEY) 
    Event code 67 (KEY_F9) 
    Event code 113 (KEY_MUTE) 
    Event code 114 (KEY_VOLUMEDOWN) 
    Event code 115 (KEY_VOLUMEUP) 
Properties: 
Testing ... (interrupt to exit) 
Event: time 1642457988.1642457988, type 1 (EV_KEY), code 114 (KEY_VOLUMEDOWN), value 1 
Event: time 1642457988.1642457988, -------------- SYN_REPORT ------------ Event: time 1642457988.1642457988, type 1 (EV_KEY), code 114 (KEY_VOLUMEDOWN), value 0 
Event: time 1642457988.1642457988, -------------- SYN_REPORT ------------
ラベル(2)
添付
100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎01-24-2022 04:46 PM
更新者: