This is the procedure and patch to set up Ubuntu 12.04 64bit Linux Host PC and building i.MX28 L2.6.35_1.1.0_130130. It has been tested to build GNOME profile and with FSL Standard MM codec.
A) Basic Requirement:
- Set up the Linux Host PC using ubuntu-12.04.3-desktop-amd64.iso
- Make sure the previous LTIB installation and the /opt/freescale have been removed
B) Installed the needed packages to the Linux Host PC
$ sudo apt-get update
$ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev
$ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool
$ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool
$ sudo apt-get install uuid-dev liblzo2-dev
$ sudo apt-get install tcl dpkg
$ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev
$ sudo apt-get install texlive texinfo
$ sudo apt-get install ia32-libs libc6-dev-i386 lib32z1
$ sudo apt-get install uboot-mkimage
$ sudo apt-get install scrollkeeper
$ sudo apt-get install gparted
$ sudo apt-get install nfs-common nfs-kernel-server
$ sudo apt-get install git-core git-doc git-email git-gui gitk
$ sudo apt-get install meld atftpd
C) Unpack and install the LTIB source package and assume done on the home directory:
$ cd ~
$ tar -zxvf L2.6.35_1.1.0_130130_source.tar.gz
$ ./L2.6.35_1.1.0_130130_source/install
After that, you will find ~/ltib directory created
D) Apply the patch to make L2.6.35_1.1.0 could be installed and compiled on Ubuntu 12.04 64bit OS
$ cd ~/ltib
$ git apply 0001_make_L2.6.35_1.1.0_130130_compile_on_ubuntu_12.04_64bit_OS.patch
a) The patch modifies the following files:
- dist/lfs-5.1/base_libs/base_libs.spec
- dist/lfs-5.1/lkc/lkc.spec
- dist/lfs-5.1/mux_server/mux_server.spec
- dist/lfs-5.1/ncurses/ncurses.spec
b) Add the following files to the pkgs directory:
- pkgs/lkc-1.4-lib.patch
- pkgs/lkc-1.4-lib.patch.md5
E) Then, it is ready to proceed the rest of the LTIB env setup process:
$ cd ~/ltib
$ ./ltib -m config
$ ./ltib
Reference:
NOTE:
When compiling gstreamer, this warning was pop up. Just ignore it seems okay.