All Boards LTIB Config Ubuntu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

All Boards LTIB Config Ubuntu

All Boards LTIB Config Ubuntu

Ubuntu distro uses dash instead of bash as shell, then change it to bash:

# cd /bin
# sudo rm sh
# sudo ln -s bash sh

Install all necessary packages by typing:

sudo apt-get install patch g++ rpm zlib1g-dev m4 bison libncurses5-dev libglib2.0-dev gettext \
build-essential tcl intltool libxml2-dev liborbit2-dev libx11-dev ccache flex uuid-dev liblzo2-dev

If under Ubuntu 64bit, install ia32-libs package:

sudo apt-get install ia32-libs
  • If you will install Xorg in your ltib, you will need to install this package:
sudo apt-get install x11proto-core-dev
  • If you will install gtk+ in your ltib, you will need to install the following packages:
sudo apt-get install libdbus-glib-1-dev libgtk2.0-dev libdbus-glib-1-dev

Configure visudo file, as root using the command "/usr/sbin/visudo", and add the following line in the User privilege section:

username ALL = NOPASSWD: /usr/bin/rpm, /opt/freescale/ltib/usr/bin/rpm

Where username is your user name, the name you use to do logon in your system.

Classic Error messages and solutions under Ubuntu

Can't exec "mconf": No such file or directory at /home/tic/ltib/bin/Ltibutils.pm line 972. exec: mconf /home/tic/ltib/config/main.lkc: No such file or directory at /home/tic/ltib/bin/Ltibutils.pm line 972. traceback:   Ltibutils::system_nb:972   main::get_plat_dir:2947     main:548 Started: Tue Feb 16 18:01:38 2010 Ended:  Tue Feb 16 18:59:26 2010 Elapsed: 3468 seconds Build Failed

Solution: edit the ltib script

line 925:

        

          # install the new package           $cmd  = "$cf->{sudo} $cf->{rpm} ";           $cmd .= "--root $cf->{rpmroot} ";           $cmd .= "--dbpath $cf->{rpmdb} ";           $cmd .= "--prefix $cf->{rpmipfx} " if $cf->{rpmipfx};           $cmd .= "--ignorearch -ivh ";           $cmd .= "--force "  unless $cf->{conflicts} || $cf->{hostinst};           $cmd .= "--replacepkgs --replacefiles " if $cf->{hostinst};           $cmd .= "--nodeps " if $cf->{nodeps};           $cmd .= "--excludedocs "; +        $cmd .= "--force-debian " if $rpm =~ m/rpm-fs/ && `uname -a` =~ m/ubuntu/i;           $cmd .= "--define '_tmppath $cf->{tmppath}' ";           $cmd .= "$rpm";


error: cannot open Name index using db3 - No such file or directory (2) error: cannot open Name index using db3 - No such file or directory (2) sudo rpm --root / --dbpath /tmp/rpm-tic/rpmdb -e --allmatches --nodeps --define '_tmppath /home/tic/ltib/tmp' rpm-fs 2>/dev/null sudo rpm --root / --dbpath /tmp/rpm-tic/rpmdb --ignorearch -ivh --force --nodeps --excludedocs --define '_tmppath /home/tic/ltib/tmp'  /tmp/rpm-tic/RPMS/i686/rpm-fs-4.0.4-1.i686.rpm rpm: please use alien to install rpm packages on Debian, if you are really sure use --force-debian switch. See README.Debian for more details. sudo /opt/freescale/ltib/usr/bin/rpm --root / --dbpath /opt/freescale/ltib/var/lib/rpm -Uv --justdb --notriggers --noscripts --nodeps  /tmp/rpm-tic/RPMS/i686/rpm-fs-4.0.4-1.i686.rpm sudo: /opt/freescale/ltib/usr/bin/rpm: command not found mkdir: cannot create directory `/opt/freescale': Permission denied Cannot create the download directory:   /opt/freescale/pkgs Either change to a global directory you have write permissions to, or create it as root.  Please set the permissions to 777 traceback:   main::check_dirs:2469   main::host_checks:1426     main:542 Started: Wed Nov 25 01:56:53 2009 Ended:  Wed Nov 25 02:07:42 2009 Elapsed: 649 seconds Build Failed

solution : sudo chmod 777 /opt


make[1]: Entering directory `/opt/freescale/ltib/usr/src/rpm/BUILD/texinfo-4.8' Making all in tools make[2]: Entering directory `/opt/freescale/ltib/usr/src/rpm/BUILD/texinfo-4.8/tools' make[2]: *** No rule to make target `all'.  Stop. make[2]: Leaving directory `/opt/freescale/ltib/usr/src/rpm/BUILD/texinfo-4.8/tools' make[1]: *** [all-recursive] Error 1 make[1]: Leaving directory `/opt/freescale/ltib/usr/src/rpm/BUILD/texinfo-4.8' make: *** [all] Error 2 error: Bad exit status from /home/tic/ltib/tmp/rpm-tmp.U8vEdX (%build) RPM build errors:     Bad exit status from /home/tic/ltib/tmp/rpm-tmp.U8vEdX (%build) Build time for texinfo: 55 seconds Failed building texinfo Died at ./ltib line 1380. traceback:   main::build_host_rpms:1380   main::host_checks:1435     main:542 Started: Wed Nov 25 20:10:43 2009 Ended:  Wed Nov 25 20:31:42 2009 Elapsed: 1259 seconds These packages failed to build: texinfo Build Failed

solution : install ccache package in host


+ cd /opt/freescale/ltib/usr/src/rpm/BUILD + cd lkc-1.4 + make -j1 conf mconf gcc -O0 -Wall -g -fPIC -c conf.c -o conf.o bison -l -b zconf -p zconf zconf.y flex -L -Pzconf zconf.l make: flex: Command not found make: *** [lex.zconf.c] Error 127 error: Bad exit status from /home/tic/ltib/tmp/rpm-tmp.010CjL (%build) RPM build errors:     Bad exit status from /home/tic/ltib/tmp/rpm-tmp.010CjL (%build) Build time for lkc: 2 seconds Failed building lkc Died at ./ltib line 1380. traceback:   main::build_host_rpms:1380   main::host_checks:1435     main:542 Started: Thu Nov 26 00:33:46 2009 Ended:  Thu Nov 26 01:19:39 2009 Elapsed: 2753 seconds These packages failed to build: lkc Build Failed

solution : install flex package in host


Making all in po make[2]: Entering directory `/home/tic/ltib/rpm/BUILD/alsa-utils-1.0.11rc2/alsaconf/po' mv: cannot stat `t-ja.gmo': No such file or directory make[2]: *** [ja.gmo] Error 1 make[2]: *** Waiting for unfinished jobs.... mv: cannot stat `t-ru.gmo': No such file or directory make[2]: *** [ru.gmo] Error 1 make[2]: Leaving directory `/home/tic/ltib/rpm/BUILD/alsa-utils-1.0.11rc2/alsaconf/po' make[1]: *** [all-recursive] Error 1 make[1]: Leaving directory `/home/tic/ltib/rpm/BUILD/alsa-utils-1.0.11rc2/alsaconf' make: *** [all-recursive] Error 1 error: Bad exit status from /home/tic/ltib/tmp/rpm-tmp.93730 (%build) RPM build errors:     Bad exit status from /home/tic/ltib/tmp/rpm-tmp.93730 (%build) Build time for alsa-utils: 84 seconds Failed building alsa-utils f_buildrpms() returned an error, exiting traceback:   main:560 Started: Sat Nov 28 07:39:40 2009 Ended:  Sat Nov 28 08:17:18 2009 Elapsed: 2258 seconds These packages failed to build: alsa-utils Build Failed Exiting on error or interrupt

solution : install package gettext and ja-trans


checking for glib-genmarshal... no configure: error: Could not find a glib-genmarshal in your PATH error: Bad exit status from /home/tic/ltib/tmp/rpm-tmp.13030 (%build) RPM build errors:     Bad exit status from /home/tic/ltib/tmp/rpm-tmp.13030 (%build) Build time for glib2: 107 seconds Failed building glib2 f_buildrpms() returned an error, exiting traceback:   main:560 Started: Sat Dec  5 03:19:36 2009 Ended:  Sat Dec  5 03:29:46 2009 Elapsed: 610 seconds These packages failed to build: glib2 Build Failed Exiting on error or interrupt

solution : install the package libglib2.0-dev

ラベル(1)
タグ(1)
コメント

Great Documentation :smileyhappy:

Thanks a lot,

Saurabh

Hi, i have this error :-(

util.c:(.text+0xa4d): undefined reference to `waddch'
util.c:(.text+0xa58): undefined reference to `winch'
util.c:(.text+0xa6c): undefined reference to `waddch'
util.c:(.text+0xa8b): undefined reference to `wnoutrefresh'
collect2: ld returned 1 exit status
make: ** [mconf] Erro 1
erro: Código de saída inválido do /home/lucas/ltib/tmp/rpm-tmp.75915 (%build)


Erros de criação do RPM:
    Código de saída inválido do /home/lucas/ltib/tmp/rpm-tmp.75915 (%build)
Build time for lkc: 3 seconds

Failed building lkc
Died at ./ltib line 1393.
traceback:
main::build_host_rpms:1393
  main::host_checks:1448
   main:554


Started: Tue May  7 17:43:23 2013
Ended:   Tue May  7 17:55:25 2013
Elapsed: 722 seconds

These packages failed to build:
lkc

Build Failed

OBS: alls packages installed correctly, but always this erro

I edited the ltib file as you said above and added the line "$cmd .= "--force-debian " if $rpm =~ m/rpm-fs/ && `uname -a` =~ m/ubuntu/i;" but it still gives the same error :

defined(@array) is deprecated at /home/sarjak/Downloads/L2.6.35_1.1.0_130130_source/yes/ltib/bin/Ltibutils.pm line 362.

    (Maybe you should just omit the defined()?)

Useless use of numeric eq (==) in void context at ./ltib line 2519.

Can't exec "mconf": No such file or directory at /home/sarjak/Downloads/L2.6.35_1.1.0_130130_source/yes/ltib/bin/Ltibutils.pm line 1006.

exec: mconf /home/sarjak/Downloads/L2.6.35_1.1.0_130130_source/yes/ltib/config/main.lkc: No such file or directory at /home/sarjak/Downloads/L2.6.35_1.1.0_130130_source/yes/ltib/bin/Ltibutils.pm line 1006.

traceback:

Ltibutils::system_nb:1006

  main::get_plat_dir:2970

   main:560

Started: Sun Mar 29 21:19:06 2015

Ended:   Sun Mar 29 21:19:06 2015

Elapsed: 0 seconds

Build Failed

Exiting on error or interrupt

Died at ./ltib line 2970.

traceback:

main::get_plat_dir:2970

  main:560

Started: Sun Mar 29 21:19:06 2015

Ended:   Sun Mar 29 21:19:06 2015

Elapsed: 0 seconds

Build Failed

Exiting on error or interrupt

sarjak@sarjak-OptiPlex-7011:~/Downloads/L2.6.35_1.1.0_130130_source/yes/ltib$

Can you please help?? It will be appreciated.

Thank you very much.

評価なし
バージョン履歴
最終更新日:
‎09-10-2020 03:34 AM
更新者: