コミュニティを検索
10-27-2025
03:11 AM
Hi,
Recently, several customers have inquired about how to program the eMMC on the RDB3 development board directly via USB in U-Boot. These customers are designing custom boards based on RDB3 w...
ラベル:
06-20-2025
01:04 PM
...Personal computer.
How to erase the eMMC?
This method will use another boot source (Micro SD) to erase the eMMC so, it is needed to flash the Micro SD with at least the bootloader (U-boot), y...
05-23-2025
05:04 PM
...able provides the boot devices supported for LP boot:
In LP boot, up to three containers (NXP and OEM containers) are expected to be handled by CM33 ROM code. • NXP container (optional): E...
06-12-2026
06:29 AM
Hello, Can you please tell me how to boot the cortex M7 from uboot? It seems that cortex a55/uboot have no access to the TCM of M7, so it is not possible to load the image. On the other hand, the M...
08-07-2026
03:20 AM
1. As shown in the figure, does the "Authenticate Image" process verify the hash value during the SHA-512 hashing stage? 2. If I set the hash value, will the BootROM verify the i...
01-19-2024
11:11 PM
2件の賞賛
Hello there.
Here is a good way to use U-boot in an efficient way with custom scripts.
The bootscript is an script that is automatically executed when the boot loader starts, and before the OS a...
05-06-2026
06:53 PM
1件の賞賛
...ebug || true
# write boot loader — this partition was set to read-only in DTS during testing, skip erase for now
# FBK: ucmd . /tmp/mtd.sh; flash_erase /dev/mtd${nandboot} 0 0
# FBK: ucp imx-boot-imx95-1...
ラベル:
11-06-2024
12:26 AM
SECURE BOOT
Secure Boot introduction
Build secure boot ATF image
Generate secure boot CSF headers for Linux tiny itb image
Deploy secure boot images on the target board
Blow OTPMK fuse i...
09-20-2024
04:45 AM
The layer attached to this article is obsolete. Please use the meta-imx-fastboot GitHub repo instead.
The purpose of this article is to show how to reduce the boot time on i.MX 8QXP u...
10-10-2014
12:20 PM
13件の賞賛