コミュニティを検索
07-08-2025
11:08 PM
NETC is a TSN capable Ethernet IP, which enables a comprehensive portfolio of Ethernet solutions. One of the major capabilities offered by NETC is the support of Time Sensitive Networking (TSN). T...
01-15-2026
03:34 AM
I need to test Time sensitive networking , IEEE 802.1AS, 802.1Qbv and 802.1Qbu, on s32g3. Should I order a reference design board (RDB3) or Evaulation board (EVB3).
09-14-2019
03:30 AM
Time Sensitive Networking(TSN) is an extension to traditional Ethernet networks, providing a set of standards compatible with IEEE 802.1 and 802.3. TSN aims to provide guarantees for deterministic l...
09-06-2018
01:17 PM
This presentation will explore key Time-Sensitive Networking (TSN) standards and how they relate to Automotive requirements. An overview of the relevant IEEE® 802.1 TSN standards will be g...
10-22-2018
04:08 PM
Time-sensitive automotive Ethernet network can increase the precision, reliability, robustness and network security of in-vehicle network and enhance the way toward autonomous driving. The NXP S...
08-15-2017
12:34 PM
Time-Sensitive Networking is the next buzz world in the industrial and automotive Ethernet domain. In this session we will dig into the TSN standards to highlight the key features that are most r...
05-21-2018
07:19 AM
1件の賞賛
Time-Sensitive Networking (TSN) makes deterministic Ethernet possible. TSN provides evolution for industrial real-time networks and is a set of IEEE® 802 Ethernet sub-standards defined by the IEEE T...
05-28-2025
05:34 AM
Realtime data transfer over Ethernet using IEEE1722 protocol – Time sensitive networking
Cílem práce je demonstrovat přenos a zpracování časově kritických signálů v reálném čase v rámci p...
ラベル:
05-25-2016
01:37 PM
Time-Sensitive Networking (TSN), a set of IEEE® 802 Ethernet sub-standards, is making deterministic Ethernet possible – especially for the automotive and industrial markets. This session will cover t...
ラベル:
06-14-2018
02:49 PM
This presentation will explore key Time-Sensitive Networking (TSN) standards and how they relate to Automotive requirements. An overview of the relevant IEEE® 802.1 TSN standards will be g...