NXP FTF 2016 - Training Presentations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP FTF 2016 - Training Presentations

Discussions

Sort by:
This paper will examine the use of an i.MX 6 IOT Gateway working together with a Cloud Services Platform (CSP), to collect and transmit data from a temperature sensor. The design options for seamless data transmission from device, to gateway, to cloud and then to a hand-held Smartphone will be considered and presented using Mentor Embedded Linux, Nucleus as well as Cloud Service Platforms.
View full article
Security is cited as one of the biggest obstacles preventing the IoT from reaching its potential. Learn how Trust Architecture in QorIQ processors can help you secure your IoT device, and provide end-to-end security for your IoT system - from the sensors to the cloud.
View full article
NXP offers commercial grade acceleration solutions for common networking applications in non-virtualized and virtualized environments. This session covers NXP’s acceleration solutions landscape on Layerscape and iNIC platforms. Layerscape provides acceleration solutions for Network and Security Applications, Switch Supplementary Applications and OpenFlow Based Applications leveraging LayerScape Accelerated Input Output Processor (LS AIOP).VortiQa-IAAS (Intelligent Application Acceleration Software) offers autonomous SSL processing (SSL termination) and SSL proxy capabilities and VortiQa-IVAS (Intelligent Virtualization Acceleration Software) offers an accelerated infrastructure for NFV (Network Functions Virtualization) to deploy and manage virtual networks and services in VNFs (Virtualized Network Function) on the QorIQ T2 based iNIC. VMM Offload is a NFV solution leveraging LS AIOP.
View full article
Virtual network functions offer a great deal of flexibility, allowing for dynamic provisioning of network services. Handling network services within a VM and meeting performance requirements can be challenging. It's essential to utilize specialized hardware accelerators to meet the desired performance targets. ODP/DPDK are becoming defacto standard for NFV abstracting the hardware accelerator interfaces from VNF applications. In order to leverage the data plane capability of underlying platform the hardware acceleration can be exposed to the VMs via proprietary interfaces through direct-assignment or standardized interfaces. In this session we discuss how we can leverage the hardware acceleration on QorIQ platforms for developing optimized virtual network functions with DPDK/ODP.
View full article
Exploration of the use cases and applications that are ideal for the DPAA2, including vCPE, UTM, the intelligent edge, Top-of-Rack switching and storage.
View full article
The AIOP C programmable packet engine is a fundamental component of the Data Path Acceleration Architecture (DPAA2). It provides customers with an opportunity to achieve the best performance per watt solution, by offloading routine packet processing tasks to the AIOP packet engine, while doing more complex processing on the ARMv8 cores. This sessions explores how customers can get to fast time-to-market with high performance, commercial grade acceleration packages from NXP.
View full article
Learn how QorIQ processors and VortiQa software are enabling solutions for iNICs Smart NICs, UTM appliances and virtualized security applications.
View full article
Review of RF Power Amplifier Fundamentals needed to find the best solutions. Watch Video Presentation
View full article
High speed internet always and everywhere is the challenge we are facing. Small cells provide the solution to fill the coverage gaps of the regular basestation infrastructure. This lecture shows the NXP high performance RF solutions to cover both the transmit and receive side of the small cells.
View full article
This session will provide tips that will help speed up silicon bring up of the QorIQ LS1043A processor.
View full article
Overview of the QorIQ LS2 and LS1088 processors, including the interfaces supported by the LS family, considerations while designing with these devices and use case examples. Watch Video Presentation
View full article
As the 5G standard is being defined, high throughput, low latency and a high number of users are among the key requirements to drive 5G services. See how NXP is blending these ingredients to design an optimal hardware architecture to address the challenges of 5G.
View full article
With exponential growth in today's cloud data centers, the demand for data storage and security is exploding. Data deduplication combined with encryption is a requirement. This session will provide an overview of how NXP has developed an innovative solution using intelligent storage accelerators without having to throw expensive cores at it. The performance-per-watt and the total cost savings of this solution are formidable. This same approach has been taken in the next-generation Software Defined Storage (SDS) platform from NXP which not only solves the data dedupe and encryption problem but also the compression, RAID and traffic offload requirement of a complete scalable SDS solution.
View full article
Learn about the exciting new Network Function Virtualization use case driving enterprise OEMs and service provider Cloud and premises architectures. Understand the new NXP open standard and optimized NFV system solutions which offers best performance-per-watt. And realize how this NFV software suite, combined with NXP processors, will protect customer CAPEX/OPEX, speed deployment time to market and enable new customer revenue streams.
View full article
Learn how QorIQ LS Series solutions are powering virtualized networking. Compelling cases will be made relative to performance (both by general purpose processor and offload capabilities – AIOP), scalability (NXP’s LS1 and LS2 solutions) and flexibility (Open NFV and Service Chaining under standard and open releases – Open Stack, Open Daylight, etc.) Watch Video Presentation
View full article
Learn how to get the most out of the PCI performance and Ethernet when designing for line rate architecture. Watch Video Presentation
View full article
Time-Sensitive Networking (TSN), a set of IEEE® 802 Ethernet sub-standards, is making deterministic Ethernet possible – especially for the automotive and industrial markets. This session will cover the advantages of TSN and current TSN standards and products. Watch Video Presentation
View full article
ARM-based processors have been designed into many cutting-edge systems thanks to a well-balanced combination of performance, feature set and power. One of the critical factors fueling innovation and time-to-market is enablement. This session will look into the enablement NXP provides and explore how Community Boards expand the range of opportunities. Bring your ideas!
View full article
A look at new types of low- or battery-powered and space-constrained applications made possible be the latest innovations in communications processors, including portable storage, IoT Gateways and embedded control.
View full article
Explore real world IoT use cases for home, healthcare and industrial applications. Includes a demo of interoperating QorIQ LS1043A gateway, Kinetis device running Thread, WiFi and NXP and 3rd party software for a secure connected solution.
View full article