コミュニティを検索
10-08-2020
09:48 AM
1件の賞賛
Overview
NXP’s Motion Control and Robotics solution provides the computing performance, embedded connectivity, low latency and a real-time open source operating system to address the r...
ラベル:
03-31-2025
11:05 PM
Attached package includes BSP patch for AI Robot Platform Based on i.MX 8M Plus
Version 6.1.55 : Rel_imx_6.1.55-2.2.0_8mp_airobot.tar.gz
10-07-2020
10:18 AM
Overview
Factory automation systems connect with each other through robust communication paths and with the user through intuitive HMIs. To meet these needs and the demand for greener, m...
ラベル:
11-20-2019
08:02 AM
...otion control and robotics space. Features High-accuracy Rot-Vector High-end PLC Industrial security gateway High-performance moto and driver Block Diagram Products Category N...
ラベル:
12-14-2020
01:38 AM
3件の賞賛
05-25-2021
09:27 PM
1件の賞賛
...o understand the advantage between them ? Could you help to share some information about the camera using in the AI Robot EVK ?
05-14-2021
02:03 AM
@xiaodong_zhang Hi Xiaodong This is KingLiu , we have already got one AI Robot EVK ,and compiled the Yocto BSP 5.4.70.2.30 source code successully . Right now I decide to use the c...
ラベル
- ラベル:
-
Linux
-
Yocto Project
返信の結果を表示(3)
-
...latbuffers are due to be built (/workdir/imx-yocto-bsp-5_10_72-2_2_0-robotics/sources/meta-robot-platform/i...
-
...9%A8%E4%BA%BA%E5%B9%B3%E5%8F%B0-i-MX-Robot-Platform/ta-p/1198619 to create a robotics image f...
-
...ources/meta-robot-platform/imx/meta-robot/recipes-devtools/python, it's context as the f...
07-19-2013
08:13 AM
15件の賞賛
A special thanks to emh203 who has worked with us to create this wonderful series of videos covering general MCU topics and more specific Freescale Cup training. We look forward to more videos ...
10-14-2019
06:38 AM
Description In this demo we show how to create a zumo robot basic controller. For this we will use the FRDM-KW41 card, an H bridge, and a cell phone with the NXP IoT toolbox application. From the a...
ラベル:
01-31-2013
02:48 PM
2件の賞賛