コミュニティを検索
09-08-2025
01:55 AM
Hello, I would like to ask how to read your company's M1 card with ST's NFC reader ST25R3920B. ST card readers support the communication of mifare-classic cards, but they don't support the e...
返信の結果を表示(5)
-
...ommunication with MIFARE Classic EV1 1K - 4K takes place according to the ISO/IEC 14443A protocol. P...
-
...ection 12.1 of the MIFARE Classic EV1 1K Data Sheet. For the authentication, one of the two secret k...
-
...UTHENTICATION part belong to ISO 14443-4? Does MIFARE Classic card support ISO14443-4? BR SLian
-
Hello I am using st25r200 reader to detect the mifare classic 4k card and perform read/write o...
-
Hello @SLianksnc, Good Day! Communication with the MIFARE Classic card is compliant with the I...
06-26-2026
06:55 AM
Hi, In my product, I use the PN5190 with NFC Lib to read different types of cards. I’m having an issue with one customer: the device reads original MIFARE Classic cards without problems, but this c...
03-25-2025
01:31 PM
...hey use Mifare Ultralight. Now they want to get access to several other Tags, e.g: Mifare® Classic®, Ultralight®, Ultralight C®, Plus®, DESFire® EV1, EV2, EV3, ICODE 2, ICODE SLI. I would choose t...
ラベル
11-27-2025
10:36 PM
In daily work, many customers are asking how to develop Mifare Desfire EV3. Yes, it is true that the Mifare Desfire EV3 is a highly secure product, and the related application documents are c...
02-25-2021
12:06 AM
Hi all, here's my problem. I am using Mifare Classic 1K. My goal would be to enter the memory of the card with the keys I know (factory default for the first time), write in the sector of my i...
11-14-2023
06:53 AM
When i investigate Mifare plus 2 and Mifare desfire ev3. I couldnt find any differences about security. I am trying to find most secure smart card. I found two of them. I understand t...
05-02-2025
01:05 PM
Hello, hope this is the correct forum to ask this... I'm planning to offer a payments product based on mifare 1k classic cards and I would like to know if there is a way to clone all the info (i...
03-18-2024
01:26 AM
Hello, So far, we've been working with Mifare Classic 1K cards, but from now on, we'll be using Mifare Plus EV2 and DESFire EV3 cards. We want to add security to our design by implementing a s...
12-19-2019
01:23 AM
...XP Before start the demonstration, please connect Pegoda with your PC via USB and place the MIFARE DESFire Light card on the reader. The history and log can be fetched from the attachment....
09-14-2022
01:43 AM
Hello, I am trying to get a Mifare Desfire EV3 tag to communicate with a PN5180. The PN5180 is connected through SPI bus to a ESP32 controller module. I am using a library from the Internet, i...
返信の結果を表示(7)
-
...elp) get ISO14443-3, ISO1444-4 and ISO7816-4 Main info is in DS487030-MF3D(H)x3 MIFARE DESFire EV3 c...
-
Hi I would suggest you refer to AN 10833: MIFARE type identification procedure. there is f...
-
Hi @c_hahn MIFARE DESFire family is secured by NDA. It means all the i...
-
...nfortunately, we can not discuss that in detail here, as MIFARE DESFire documentation is only provided via NDA....
-
...it. I am only targeting MIFARE Desfire EV3 tags (maybe I will use the EV1 compatibility mode, b...
-
I found the root cause for the problems with talking to the MIFARE Desfire EV3: After successful c...
-
...here is also a MIFARE DESFire abstraction layer (phalMfdf.h) where you simply can call whatever c...