Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
19,462 results
Sorted by:
10-27-2025
03:11 AM
Hi,
Recently, several customers have inquired about how to program the eMMC on the RDB3 development board directly via USB in U-Boot. These customers are designing custom boards based on RDB3 w...
Labels:
06-20-2025
01:04 PM
...Personal computer.
How to erase the eMMC?
This method will use another boot source (Micro SD) to erase the eMMC so, it is needed to flash the Micro SD with at least the bootloader (U-boot), y...
05-23-2025
05:04 PM
...able provides the boot devices supported for LP boot:
In LP boot, up to three containers (NXP and OEM containers) are expected to be handled by CM33 ROM code. • NXP container (optional): E...
05-20-2026
12:50 AM
Hello, I'm trying to boot from a SPI NAND on i.MX8ULP. The evk has a SPI NOR attached and I was able to boot from it, but when trying with a NAND on our boards I cannot get this to work. I've c...
Show results in replies (4)
-
...anual states that booting from an SPI NAND connected to FlexSPI2 is supported. However, we are c...
-
Hi @Rita_Wang Are there any updates on this inquiry? If booting from SPI NAND is not s...
-
I got access to the Golden Shiny Oscilloscope™ and could confirm that, booting in that c...
-
Hi @Rita_Wang I received information that SPI NAND boot is supported with the same s...
05-06-2026
06:53 PM
1 Kudo
...yte(s) (64 page(s)) at offset 0x00000000
u-boot=> booti ${loadaddr} - ${fdt_addr} ------------------>read kernel, dtb in NAND
## Flattened Device Tree blob at 93000000
Booting using the fdt b...
Labels:
01-19-2024
11:11 PM
2 Kudos
Hello there.
Here is a good way to use U-boot in an efficient way with custom scripts.
The bootscript is an script that is automatically executed when the boot loader starts, and before the OS a...
11-06-2024
12:26 AM
SECURE BOOT
Secure Boot introduction
Build secure boot ATF image
Generate secure boot CSF headers for Linux tiny itb image
Deploy secure boot images on the target board
Blow OTPMK fuse i...
09-20-2024
04:45 AM
The layer attached to this article is obsolete. Please use the meta-imx-fastboot GitHub repo instead.
The purpose of this article is to show how to reduce the boot time on i.MX 8QXP u...
10-10-2014
12:20 PM
13 Kudos
09-30-2022
09:11 AM
In the i.MX8MP support 3 SDIO interface, and in the reference board i.MX 8M Plus LPDDR4 EVK design default use the eMMC connect to the USDHC3 to boot up from emmc,use the SD card connect to the U...