After setting up an Yocto build environment as described in the L4.19.35_1.0.0 BSP Yocto Project User's Guide, apply the attached patch to the meta-fsl-bsp-release layer:
<yocto_dir>/sources/meta-fsl-bsp-release$ git am eiq-sample-apps-Add-recipe.patch
To include the applications in the image, add the following line to local.conf:
IMAGE_INSTALL_append += "eiq-sample-apps"
This will include all applications from the eIQ Sample Apps repository to the built image.
Hello:
I encounter a error when applied the attached patch.
ERROR: Nothing RPROVIDES 'eiq-sample-apps' (but /home/duxy/fsl-arm-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/dynamic-layers/qt5-layer/recipes-fsl/images/fsl-image-qt5.bb RDEPENDS on or otherwise requires it)
NOTE: Runtime target 'eiq-sample-apps' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['eiq-sample-apps']
ERROR: Required build target 'fsl-image-qt5' has no buildable providers.
Missing or unbuildable dependency chain was: ['fsl-image-qt5', 'eiq-sample-apps']
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
how to resolve it? Before applied the patch, I have compiled the eIQ image successfully.
Hi coindu,
Could you please confirm that the patch was successfully applied? Does the eiq-sample-apps folder exists in meta-fsl-bsp-release/imx/meta-ml/recipes-apps/eiq-sample-apps? What BSP release are you using?
Thanks!
Vanessa
fsl-arm-yocto-bsp/sources/meta-fsl-bsp-release$ git log
commit 7a67a5a9f8bb31a50bf6704d6383957c8264c656
Author: Vanessa Maegima <[email protected]>
Date: Tue Oct 1 16:07:22 2019 -0300
eiq-sample-apps: Add recipe
Recipe to deploy all eiq_sample_apps to an iMX8* board.
Signed-off-by: Vanessa Maegima <[email protected]>
commit 8eeb420fad668b733ab95b460895e1c337c66b25
Author: Neena Busireddy <[email protected]>
Date: Fri May 3 10:50:12 2019 -0500
vkmark: Use SHA in SRCREV instead of AUTOREV
Signed-off-by: Neena Busireddy <[email protected]>
I reference 《UM11226.pdf》 to set the environment
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.0.0_machinelearning.xml$: EULA=1 MACHINE=imx8mqevk DISTRO=fsl-imx-xwayland source ./fsl-setup-release.sh -b build-xwayland $: echo "BBLAYERS += \" \${BSPDIR}/sources/meta-imx-machinelearning \"" >> conf/bblayers.confmeta-imx-machinelearning/recipes-libraries/tensorflow/tensorflow_1.12.0.bb modify
COMPATIBLE_MACHINE = "(imx8qm|imx8mq|imx8mm)"bitbake fsl-image-qt5
Could you please modify the COMPATIBLE_MACHINE in the eiq_sample_apps recipe as you did for TensorFlow and let me know how it goes?
COMPATIBLE_MACHINE = "(imx8qm|imx8mq|imx8mm)"My patch applies on top of a newer release L4.19.35 but let's try to make this work on L4.14.98
It do not work to modify COMPATIBLE_MACHINE.
It doesn't matter, I still compile according to the documentation
Please try adding the following line to conf/bblayers.conf:
BBLAYERS += " ${BSPDIR}/sources/meta-fsl-bsp-release/imx/meta-ml "
Hi
The Yocto Project User's Guide say that eIQ is integrated in meta-eiq, but this layer doesn't exist.
There is a meta-ml: is ti the same thing?
Philippe
Hi philippemidol-monnet,
Yes, you are correct. I will ask for this to be updated.
Thanks for reporting.
Vanessa