Window Covering Server Cluster

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Window Covering Server Cluster

Jump to solution
4,324 Views
nguyenanhgiau10
Contributor IV

Hi all,

I am developing a smart curtain device. It use Window Covering Server Cluster.

But I see something wrong with this cluster in "ZigBee Cluster Library Specification".

Window Covering Information Attribute Set and Window Covering Setting Attribute Set use the same attribute ID.

pastedImage_1.png

pastedImage_2.png

I think it should be:
Window Covering Information Attribute Set: 0x0000 - 0x000F
Window Covering Setting Attribute Set: 0x0010 - 0x001F

Can you explain it?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
4,238 Views
nguyenanhgiau10
Contributor IV
0 Kudos
Reply
3 Replies
3,927 Views
dmsherazi
Contributor IV

Hi,

Did you manage to add the Window Covering Server Cluster for NXP? I am trying to add it to our Gateway /Control Bridge. Can you let me know the steps to follow and possibly share the code that will help me?

0 Kudos
Reply
4,238 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Giau.

The server attributes for the Windows Covering has an Attribute Set depending on the description that you want, in this case.

pastedImage_1.png

Hope it helps.

Regards,

Mario

0 Kudos
Reply
4,239 Views
nguyenanhgiau10
Contributor IV

Hi mario_castaneda 

I got it.
pastedImage_2.png
Thanks!

0 Kudos
Reply