Trap error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trap error

2,652 Views
qidongli
Contributor II

I use JN-AN-1218-Zigbee-3-0-Light-Bulb smaple compile occur error message:

!!! Trap error
u32PICMR = 0 : u32PICSR = 8000
u32PICMSR = 0 : u32IPMR = 0
u32IHPR = c : u32AINT = 8000 u32PINT 0
EPCR = b3f60 : EEAR = 9cffefff

In Application I use eZLO_RegisterOnOffLightEndPoint() function register four application endpoint,then,download program to evaluation boards, occur above error message, how to solve this problem,And without changing the requirements!

Thanks!

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,480 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

Could you please provide the AN and the SDK version that you are working on?

Regards,

Mario

0 Kudos
Reply

2,480 Views
qidongli
Contributor II

The ZStack SDK Version is JN-SW-4170 Zigbee 3.0 v1840, The Project sample is JN-AN-1218-Zigbee-3-0-Light-Bulb. You have ways solve this question?

0 Kudos
Reply

2,480 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

Did you try the example with any modification?

Could you please provide what did you modify?

Regards,

Mario

0 Kudos
Reply