Problems setting up Beyondstudio for NXP IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems setting up Beyondstudio for NXP IDE

19,479 Views
martinpannenbae
Contributor II

Hello,

I'm new to developing ZigBee Applications and already get stuck with setting up the IDE. I have JN5168-M00 module and want to start programming with the JN-AN-1217-Zigbee-3-0-Base-Device Demo.

I installed the IDE as explained in JN-UG-3098 with BeyondStudio for NXP first, then the JN-SW-4170 Zigbee 3.0 SDK and installed the ZigBee Plugins. So far, so good.

After importing the Demo Project and trying to compile, I get a lot of symbol could not be resolved errors.Dependencies.jpg

To solve this problem I right clicked on the Project, chose Properties and then added the include files manually like shown in this picture:

Add_Includes.JPG

Many Errors vanished, but some are still there as shown here

Dependencies2.JPG

As I don't know if I'm on the right way to solve the Errors I want to ask here for some help.

Would be great if someone here can help me.

With best regards

Martin Pannenbäcker

73 Replies

10,179 Views
dheeraj_s
Contributor I

Hi 

I'm new to developing ZigBee Applications. i have download JN-AN-1217-Zigbee-3-0-Base-Device Demo code , my proplem is when i built code any of i got error "make: *** No rule to make target `all'. Stop". 

how to solve this please i tryed every thing but not solved this error.

0 Kudos
Reply

10,179 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dheeraj,

Could you please look at the next document.

https://community.nxp.com/docs/DOC-340028 

Regards,

Mario

0 Kudos
Reply

10,179 Views
adamjacob
Contributor II

Calling the makers and experts interested in using Zigbee via NXP JN5168 modules, please join the facebook group so we can help each other:)
https://goo.gl/DeYbC6
Cheers

0 Kudos
Reply

10,181 Views
dheerajsawant
Contributor V

Hello Mario Ignacio Castaneda Lopez

Thank You for your time. 

now i have resolve all issue and error. 

i resolve those issue by installing SDK of 4168.

but last error is remaining. i have take screen shot please check it. 

I think that issue is not regarding example/applicatoin, i think i am doing mistake in beyond studio setting. 

please check screen shot and give me right direction.

Thank You for your reply and your time

Untitled1.pngUntitled2.pngUntitled3.pngUntitled4.pngUntitled5.png

Thank You very much

Dheeraj Sawant

0 Kudos
Reply

10,178 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dheeraj,

It will be nice, if you can tell me what is this Application note that are working on.

Best Regards,

Mario

0 Kudos
Reply

10,181 Views
dheerajsawant
Contributor V

Hello Mario, 

our main application is related to RF based(we have to send temp reading from one module to another module). But in our office no one used beyond studio or eclipse yet. 

so i am going to familiar with this studio(Beyond Studio). 

so just for an example i am trying to compile  2 - 3 application. so right now i am compiling 

"JN-AN-1162-JenNet-IP-Smart-Home" based application. 

OR 

i request you, if you have any example/Application which i can directly import and compile(without error and with bin file to upload on controller), then please provide me.

Thank You for your time.

0 Kudos
Reply

10,181 Views
dheerajsawant
Contributor V

Hello  Mario Ignacio Castaneda Lopez,

Thank You for your time.

i am trying to compile JN-AN-1162 application. 

in that   Common -->Source-->uart.c

This application i am trying to compile. 

0 Kudos
Reply

10,181 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dheeraj,

Do you still have problems with this AN?

Best Regards,

Mario

0 Kudos
Reply

10,181 Views
dheerajsawant
Contributor V

Hello @Mario Ignacio Castaneda Lopez ,

Yes Problem is solved. 

Binary files are created by building project but error are occurring.

No there is no problem with "AN".

Sir i have another question can i get your help regarding RF communication between two JN5168 Module.

i need some information about it and if there are sample program for this communication. 

Even i have created another topic.

 

Thank You for your time.

0 Kudos
Reply

10,181 Views
dheerajsawant
Contributor V

Hello mario_castaneda‌,

i am facing a problem .

not able to upload code in Jn5168 module.

i have attached screen shot showing error that "Failed to read chip details".

Connection is  "system--Moxa cable--interfacing board(RS232)--jn5168 Module board"

error.png

Thank You for your time.

0 Kudos
Reply

10,181 Views
dheerajsawant
Contributor V

Hello,

I think Beyond studio is not detecting Moxa cable which is usb to serial converter. 

when i connect only moxa cable to system and try to check program device on Beyond studio then its started to show this error.

is there any solution?

Thank you for your time.

0 Kudos
Reply

10,181 Views
davidashraf
Contributor V

This error means either there's a problem in your connections to the module or a problem with USB driver 
If you're sure of the drivers then check your connections 
In programming mode The connection should be :
Tx -> Rx 
Rx -> Tx 
VDD -> 3.3v
GND -> 0v
SPIMISO -> GND

Notes:
-IF you're using another source of power other than USB then make sure both grounds are connected 
-After making these connections reset the module by putting RESET pin -> GND then move it back to -> VDD 
-Make Sure you're using UART0

Regards

0 Kudos
Reply

10,181 Views
dheerajsawant
Contributor V

Hello davidashraf‌,

yes connection is same as tx-rs and likewise.

Ground is common.

RESET pin -> GND then move it back to -> VDD ---its also done

using UART0(DIO9-10)pin of Jn5168 Module.

SPIMISO -> GND--------done

error1.png

but still showing same error.

0 Kudos
Reply

10,179 Views
davidashraf
Contributor V


It's DIO6-7 not (DIO9-10) 
please check it and try again and tell me 

0 Kudos
Reply

10,179 Views
dheerajsawant
Contributor V

Hello davidashraf‌,

I am really really sorry for this mistake.

yes its DIO6-7, by mistaken wrote those Digital Input and Output.

DIO9-10 are for crystal IN & OUT respectively. 

But sir still i am facing same problem. 

i have attached external crystal of 32MHz and tried to check waveform on oscilloscope but its inaccurate. 

waveform should be accurate know? "what do i do?"

i have solder 15pf capacitor as per PDF.

simultaneously i am trying to upload code from boot loading lets see what happen? 

Thank You

0 Kudos
Reply

10,179 Views
davidashraf
Contributor V

Okay 
What baud rate do you use when trying to program the module ? 
Also please Connect the module to usb then check device drivers in windows and show me what shows in usb section 

0 Kudos
Reply

10,179 Views
dheerajsawant
Contributor V

Hello davidashraf‌,

today i try something new. i tried to see data on Serial Port Monitor. 
I download Serial Port Monitor Software and see below data.

this is information of Serial Port Monitor.

i am getting this read and write values while i am programming device.

i hope you understand.


how i do this:
1) i select com port and select "dataView" from available processing tab in serial port monitor.
2) and start process.
3)open beyond studio and program device and upload program and its failed as usually.
4)open Serial Port Monitor and see below data.

i hope you understand.

Really thanks for your time.

SerialMonitor_log1.png

SerialMoniter-Log2.png

I hope you understand.

Thank you

0 Kudos
Reply

10,179 Views
dheerajsawant
Contributor V

Hi 

I think i forget to tell you , I am using  JN-AN 1162 APPLICATION. 

AND I AM TRYING UART COMMUNICATION IN DeviceRemote.c file. In main function.

0 Kudos
Reply

10,179 Views
dheerajsawant
Contributor V

Hello davidashraf‌,

Is there other tool to download binary code into JN5168 Module?

& why its Failed to read chip details on COMPORT?

Thank You

0 Kudos
Reply

10,179 Views
dheerajsawant
Contributor V

Hello davidashraf‌,

I tried different different  baud rate.

Device manager:

Device_manager.png 

Thank You 

0 Kudos
Reply