KW41Z mesh usage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KW41Z mesh usage

2,227 次查看
evgenyerlihman
Contributor IV

Hello,

I am evaluating the KW41Z chip using FRDM-KW41Z board. All the examples talk about having the commissioner as a node in the mesh. It is also said that the commissioner instantiates a node with hardcoded ID == 0x1, and that every node must have a unique ID. Can i understand that currently, NXP does not provide any way of commissioning nodes to the mesh by an outside device such as Android/iOS device? And that i cannot have more that one commisioner in the mesh (because it instantiates ID == 0x1 node) ?

Thanks,

Evgeny 

标签 (2)
3 回复数

1,800 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Evgeny,

Unfortunately, We do not have a specific app for BLE mesh, but you could implement wireless UART, create another connection and send to the phone all the data that you want.

Yes, The Mesh Commissioner application instantiates a node with the mesh address 0x0001. This address is fixed inside the library and cannot be changed from the application.

Hope it helps,

Mario

1,800 次查看
evgenyerlihman
Contributor IV

Hi Mario,

According to this: https://community.nxp.com/thread/445287 

I cant use BLE Mesh and BLE, so if i want to communicate using wireless UART with a node/commissioner. It cant be part of the Mesh at the same time?

Thanks,

Evgeny

0 项奖励
回复

1,800 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Every,

I'm sorry, I was confused, you can't use the wireless UART and be part of the mesh at the same time. You can use the mesh commissioner example and control the network through the terminal.

Best Regards,

Mario

0 项奖励
回复