KW41Z BLE IPv6 + iPhone support?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW41Z BLE IPv6 + iPhone support?

4,178件の閲覧回数
AlexJLennon
Contributor III

Hi,

I'm using the KW41Z and am reading that I should be able to use Bluetooth BLE with IPv6.

I am also reading that recent iPhones support IPv6 over BLE.

I  have run the IPv6 node example on the KW41Z but cannot seem to ping an iPhone.

Can anybody tell me if this is in fact possible?

Thanks,

Alex Lennon

ラベル(2)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

3,669件の閲覧回数
teleworm
Contributor I

Thanks for the guideline it's really an awesome work by your side. because I am looking like the same that you shared in here. I am already discussed with the iPhone ex[ert team by dialing iPhone Customer Service Number for instant help.

0 件の賞賛
返信

3,669件の閲覧回数
mariush
NXP Employee
NXP Employee

Hi Alex,

What feature and API of IOS are you using to test this? Do you have an specific app?

Regards,

Marius

0 件の賞賛
返信

3,669件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Could you please check this thread: https://community.nxp.com/thread/460511  to see if it works for you.? 

Best regards, 
Estephania 

0 件の賞賛
返信