Need more details about bool_t zps_bGetFlashCredential(uint64 u64IeeeAddr,AESSW_Block_u* puKey,uint16 *pu16Index,bool_t bTcCred,bool_t bUpdate );

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need more details about bool_t zps_bGetFlashCredential(uint64 u64IeeeAddr,AESSW_Block_u* puKey,uint16 *pu16Index,bool_t bTcCred,bool_t bUpdate );

1,406 Views
panjun
Contributor III

bool_t zps_bGetFlashCredential(uint64 u64IeeeAddr,AESSW_Block_u* puKey,uint16 *pu16Index,bool_t bTcCred,bool_t bUpdate );

bool_t bTcCred: Mean?

bool_t bUpdate:Mean?

Would you please give me more detail as above two arguments!

0 Kudos
Reply
2 Replies

1,225 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Pan,

The code is checking if the credential is present roll back to confirm that key is used and not install code.

Regards,

Mario

0 Kudos
Reply

1,225 Views
panjun
Contributor III

Through my question please Moderators ,my project is very tight and I need answers urgently!

0 Kudos
Reply