KW41Z BLE IPv6 + iPhone support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW41Z BLE IPv6 + iPhone support?

4,137 Views
AlexJLennon
Contributor III

Hi,

I'm using the KW41Z and am reading that I should be able to use Bluetooth BLE with IPv6.

I am also reading that recent iPhones support IPv6 over BLE.

I  have run the IPv6 node example on the KW41Z but cannot seem to ping an iPhone.

Can anybody tell me if this is in fact possible?

Thanks,

Alex Lennon

Labels (2)
Tags (4)
0 Kudos
Reply
3 Replies

3,628 Views
teleworm
Contributor I

Thanks for the guideline it's really an awesome work by your side. because I am looking like the same that you shared in here. I am already discussed with the iPhone ex[ert team by dialing iPhone Customer Service Number for instant help.

0 Kudos
Reply

3,628 Views
mariush
NXP Employee
NXP Employee

Hi Alex,

What feature and API of IOS are you using to test this? Do you have an specific app?

Regards,

Marius

0 Kudos
Reply

3,628 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Could you please check this thread: https://community.nxp.com/thread/460511  to see if it works for you.? 

Best regards, 
Estephania 

0 Kudos
Reply