JN5179:Load Binary File into Flash Memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JN5179:Load Binary File into Flash Memory

2,788 次查看
wupengfei
Contributor II

$ JN51xxProgrammer.exe -s COM3  -f AN1211_154_EndD_JN5179.bin

----- Error:reading chip ID-check cabling and power

 Failed to read chip details on COM3

4 回复数

2,205 次查看
davidashraf
Contributor V

Hello wupengfei‌ 
You may want to have a look here 
https://community.nxp.com/thread/460072 

Regards

0 项奖励
回复

2,205 次查看
wupengfei
Contributor II

thinks for your help ,I am following your instructions to achieve it。

2,205 次查看
davidashraf
Contributor V

wupengfei‌ 
You are welcome 
Please If it worked with you mark it as correct and helpful for others searching on the same problem find the solution easily 
If not , comment with any other solution you found to edit and modify the document.

Thanks and Regards

0 项奖励
回复

2,205 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Pengflei,

Could you please check the in the device manager that the JN5179 driver is installed correctly?

Also, if this a custom board make sure you connect the  RX of programmer to TX of module and vice versa
VDD, GND,  SPIMISO  to Ground,  RESET to Ground then 3.3v.

Please let me know your findings.

Best Regards,

Mario