JN5179:Load Binary File into Flash Memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5179:Load Binary File into Flash Memory

3,933 Views
wupengfei
Contributor II

$ JN51xxProgrammer.exe -s COM3  -f AN1211_154_EndD_JN5179.bin

----- Error:reading chip ID-check cabling and power

 Failed to read chip details on COM3

4 Replies

3,350 Views
davidashraf
Contributor V

Hello wupengfei‌ 
You may want to have a look here 
https://community.nxp.com/thread/460072 

Regards

0 Kudos
Reply

3,350 Views
wupengfei
Contributor II

thinks for your help ,I am following your instructions to achieve it。

3,350 Views
davidashraf
Contributor V

wupengfei‌ 
You are welcome 
Please If it worked with you mark it as correct and helpful for others searching on the same problem find the solution easily 
If not , comment with any other solution you found to edit and modify the document.

Thanks and Regards

0 Kudos
Reply

3,350 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Pengflei,

Could you please check the in the device manager that the JN5179 driver is installed correctly?

Also, if this a custom board make sure you connect the  RX of programmer to TX of module and vice versa
VDD, GND,  SPIMISO  to Ground,  RESET to Ground then 3.3v.

Please let me know your findings.

Best Regards,

Mario