JN5179:Load Binary File into Flash Memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5179:Load Binary File into Flash Memory

3,931件の閲覧回数
wupengfei
Contributor II

$ JN51xxProgrammer.exe -s COM3  -f AN1211_154_EndD_JN5179.bin

----- Error:reading chip ID-check cabling and power

 Failed to read chip details on COM3

4 返答(返信)

3,348件の閲覧回数
davidashraf
Contributor V

Hello wupengfei‌ 
You may want to have a look here 
https://community.nxp.com/thread/460072 

Regards

0 件の賞賛
返信

3,348件の閲覧回数
wupengfei
Contributor II

thinks for your help ,I am following your instructions to achieve it。

3,348件の閲覧回数
davidashraf
Contributor V

wupengfei‌ 
You are welcome 
Please If it worked with you mark it as correct and helpful for others searching on the same problem find the solution easily 
If not , comment with any other solution you found to edit and modify the document.

Thanks and Regards

0 件の賞賛
返信

3,348件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Pengflei,

Could you please check the in the device manager that the JN5179 driver is installed correctly?

Also, if this a custom board make sure you connect the  RX of programmer to TX of module and vice versa
VDD, GND,  SPIMISO  to Ground,  RESET to Ground then 3.3v.

Please let me know your findings.

Best Regards,

Mario