How to map values of Output Power in Connectivity Test Application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to map values of Output Power in Connectivity Test Application

跳至解决方案
1,629 次查看
vishnubeema
Contributor III

Hello,

In SMAC “Kinetis SMAC Demo Applications User's Guide.pdf” under “Chapter 4 Kinetis Connectivity Test Application” there is an option to change the output power value. But its mentioned to see corresponding reference manual. From where I can find this mapping between the register value and the converted dBm value.

 

  • ‘s’ : decrements output power value. If output power is at minimum and this key is pressed, the output power will go to maximum (in this case 0x1C). These are not directly mapped to dBm values. Instead the output power value is written to the appropriate register. The user should consult the reference manual to determine the relationship between selected value and power in dBm.

Thanks & Regards

Vishnu Beema

标记 (3)
0 项奖励
回复
1 解答
1,514 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Additionally, you can check the Data Sheet on page 27 for further information. 

Best Regards, 

Estephania 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,515 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Additionally, you can check the Data Sheet on page 27 for further information. 

Best Regards, 

Estephania 

0 项奖励
回复