How to map values of Output Power in Connectivity Test Application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to map values of Output Power in Connectivity Test Application

ソリューションへジャンプ
1,572件の閲覧回数
vishnubeema
Contributor III

Hello,

In SMAC “Kinetis SMAC Demo Applications User's Guide.pdf” under “Chapter 4 Kinetis Connectivity Test Application” there is an option to change the output power value. But its mentioned to see corresponding reference manual. From where I can find this mapping between the register value and the converted dBm value.

 

  • ‘s’ : decrements output power value. If output power is at minimum and this key is pressed, the output power will go to maximum (in this case 0x1C). These are not directly mapped to dBm values. Instead the output power value is written to the appropriate register. The user should consult the reference manual to determine the relationship between selected value and power in dBm.

Thanks & Regards

Vishnu Beema

タグ(3)
0 件の賞賛
返信
1 解決策
1,457件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Additionally, you can check the Data Sheet on page 27 for further information. 

Best Regards, 

Estephania 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,458件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Additionally, you can check the Data Sheet on page 27 for further information. 

Best Regards, 

Estephania 

0 件の賞賛
返信