How to map values of Output Power in Connectivity Test Application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to map values of Output Power in Connectivity Test Application

Jump to solution
1,574 Views
vishnubeema
Contributor III

Hello,

In SMAC “Kinetis SMAC Demo Applications User's Guide.pdf” under “Chapter 4 Kinetis Connectivity Test Application” there is an option to change the output power value. But its mentioned to see corresponding reference manual. From where I can find this mapping between the register value and the converted dBm value.

 

  • ‘s’ : decrements output power value. If output power is at minimum and this key is pressed, the output power will go to maximum (in this case 0x1C). These are not directly mapped to dBm values. Instead the output power value is written to the appropriate register. The user should consult the reference manual to determine the relationship between selected value and power in dBm.

Thanks & Regards

Vishnu Beema

0 Kudos
Reply
1 Solution
1,459 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Additionally, you can check the Data Sheet on page 27 for further information. 

Best Regards, 

Estephania 

View solution in original post

0 Kudos
Reply
1 Reply
1,460 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Additionally, you can check the Data Sheet on page 27 for further information. 

Best Regards, 

Estephania 

0 Kudos
Reply