How to check QN9083 BLE stack version?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to check QN9083 BLE stack version?

Jump to solution
5,263 Views
wang_barry
Contributor III

Hello

I want to know that how to check QN9080 BLE stack version. is BLE5.0?

 My environment:

  Hardware: QN9080 DK -V1.3

  IDE: MCUXpresso IDE 

  SDK:SDK_2.x_QN908x 2.2.6

 but I can't find the label of BLE stack on SDK 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
5,212 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @wang_barry,

The BLE 5.0 in the QN9080 is only compliance with the mandatory erratas and the optional features are not supported.

BR,

Alexis Andalon

View solution in original post

0 Kudos
Reply
4 Replies
5,236 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @wang_barry,

When you download the SDK you can find the following option:

Alexis_A_0-1648163455842.png

In the following path you can find the release notes:

SDK_2_2_6_QN908XCDK_doc.zip\docs\wireless\Bluetooth

BR,

Alexis Andalon

0 Kudos
Reply
5,230 Views
wang_barry
Contributor III

Hello @Alexis_A 

 

Thank you for the reply.

I check the release note.

The host & controller feature is BLE 5.0.

But I am not sure that all the features in this stack fulfill the BLE SIG 5.0 specification and get the certification?

0 Kudos
Reply
5,213 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @wang_barry,

The BLE 5.0 in the QN9080 is only compliance with the mandatory erratas and the optional features are not supported.

BR,

Alexis Andalon

0 Kudos
Reply
5,186 Views
wang_barry
Contributor III

Hello @Alexis_A 

 

Got it, thank you for the replay~

 

Best Regards,

Barry

0 Kudos
Reply