QN9020 fail to download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN9020 fail to download

Jump to solution
3,798 Views
Doomer
Contributor II

Hi

I managed to download the bin file under \BinFiles\BinFiles_B2_v40 from ISP

But after I download the keil built bin file from ISP or directly download from keil(using code under \Projects\BLE), the board isn't working properly, leds off and no response pushing the buttons.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,736 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me confirm you are using Bluetooth LE version 4.2? You will need to be sure to be using the qn9020b4_lib_peripheral_v42.a library

 

Regards,

 

View solution in original post

0 Kudos
Reply
7 Replies
3,765 Views
Doomer
Contributor II

I think I have correctly set the options in keil, but the board still failed to work properly.

0 Kudos
Reply
3,752 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please provide more details on which example are you using ? Are you using the low power capabilities ?

 

Regards,
Estephania

0 Kudos
Reply
3,749 Views
Doomer
Contributor II

The broadcaster example. I didn't change the code.

0 Kudos
Reply
3,737 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me confirm you are using Bluetooth LE version 4.2? You will need to be sure to be using the qn9020b4_lib_peripheral_v42.a library

 

Regards,

 

0 Kudos
Reply
3,705 Views
Doomer
Contributor II

I repaired the SDK and finally solved the problem.

Thanks a lot.

0 Kudos
Reply
3,729 Views
Doomer
Contributor II

Under QN902x_SDK_1.4.0\Projects\BLE\src\lib, I can only find qn9020b0_lib_peripheral,qn9020b1_lib_peripheral and qn9020b2_lib_peripheral for keil and IAR.

0 Kudos
Reply