How to check QN9083 BLE stack version?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to check QN9083 BLE stack version?

ソリューションへジャンプ
7,332件の閲覧回数
wang_barry
Contributor III

Hello

I want to know that how to check QN9080 BLE stack version. is BLE5.0?

 My environment:

  Hardware: QN9080 DK -V1.3

  IDE: MCUXpresso IDE 

  SDK:SDK_2.x_QN908x 2.2.6

 but I can't find the label of BLE stack on SDK 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
7,281件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @wang_barry,

The BLE 5.0 in the QN9080 is only compliance with the mandatory erratas and the optional features are not supported.

BR,

Alexis Andalon

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
7,305件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @wang_barry,

When you download the SDK you can find the following option:

Alexis_A_0-1648163455842.png

In the following path you can find the release notes:

SDK_2_2_6_QN908XCDK_doc.zip\docs\wireless\Bluetooth

BR,

Alexis Andalon

0 件の賞賛
返信
7,299件の閲覧回数
wang_barry
Contributor III

Hello @Alexis_A 

 

Thank you for the reply.

I check the release note.

The host & controller feature is BLE 5.0.

But I am not sure that all the features in this stack fulfill the BLE SIG 5.0 specification and get the certification?

0 件の賞賛
返信
7,282件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @wang_barry,

The BLE 5.0 in the QN9080 is only compliance with the mandatory erratas and the optional features are not supported.

BR,

Alexis Andalon

0 件の賞賛
返信
7,255件の閲覧回数
wang_barry
Contributor III

Hello @Alexis_A 

 

Got it, thank you for the replay~

 

Best Regards,

Barry

0 件の賞賛
返信