DUAL PAN / KW24D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DUAL PAN / KW24D

2,255 Views
mattiastörnblad
Contributor II

Hello,

As I understand it, KW24D has possibilty to do dual PAN connections! Does that mean it might be possible to run zigbee and thread at the same time, and if it is, will you provide some samples on how to do it? Another thing I would like to see is a GCC version of Zigbee stack för KW24D.

Best Regards,

Mattias Törnblad

0 Kudos
Reply
1 Reply

1,903 Views
jc_pacheco
NXP Employee
NXP Employee

Hello Mattias, 

KW2xD supports Dual PAN. The current ZigBee support for KW2xD is BeeStack 5.0.0 which contains some DualPAN ZigBee demos.

The BeeStack 5.0.0 framework is not compatible with the latest Connectivity Software for KW2xD (SMAC, MAC, Thread) available in the MKW2xD_Connectivity Software which is KSDK based.

We are working to enable ZigBee 3.0 stack in the upcoming months for MKW41Z. The Connectivity Software for KW41Z supports multiple stacks: SMAC, MAC, Thread, BLE, GFSK and ZigBee (upcoming).

Hope this helps.

-JC

0 Kudos
Reply