Importing existing projects inKDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Importing existing projects inKDS

2,295件の閲覧回数
marbro1965
Contributor I

Hi,

I want to start a new project for R41Z evaluation kit and for this I import an existing project.

Is there any way to import a project and not to have linked files but their copy in my workspace?

Best Regards

0 件の賞賛
返信
3 返答(返信)

2,160件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi marbro1965

If you are using MKW41Z_ConnSw_1.0.2, You can clone the example projects with project cloner tool. You should find it in the default path: C:\nxp\MKW41Z_ConnSw_1.0.2\tools\wireless\ProjectCloner


Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,160件の閲覧回数
marbro1965
Contributor I

I exactly did this operaction but when i open the cloned project the files

are linked files,

not copies to work directory.

Regards

2017-01-23 19:31 GMT+01:00 jorge_a_vazquez <[email protected]>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Importing existing projects inKDS

reply from Jorge Antonio Alcala Vazquez

<https://community.nxp.com/people/jorge_a_vazquez?et=watches.email.thread>

in Wireless Connectivity - View the full discussion

<https://community.nxp.com/message/870862?commentID=870862&et=watches.email.thread#comment-870862>

0 件の賞賛
返信

2,160件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi marbro1965

It will copy the files from wireless connectivity software and place it in your project, but at the moment to call them, these files are linked. You can modify them now, and your original files inside the connectivity software will not be affected (cause you have now copy).

Best Regards

Jorge Alcala

0 件の賞賛
返信