Wi-Fi® + Bluetooth® + 802.15.4 Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wi-Fi® + Bluetooth® + 802.15.4 Knowledge Base

Discussions

Sort by:
If you are trying to flash your FRDM-RW612 and one of the following J-Link errors appears: Error 1: ****** Error: Verification failed @ address 0x18000000 Error while programming flash: Verify failed.   Error 2:  ****** Error: Verification failed @ address 0x08000000 Error while programming flash: Verify failed.   This can happen because of different reasons; the one I have addressed is when we flash a RD-RW612-BGA binary into FRDM-RW612. When doing this the board will get locked, and we will no longer be able to write data into the flash until we unlock it.  Please try the following:  1. Get MCUXpresso Secure Provisioning Tool 2. Create a New Workspace and select RW612 3. In Source executable image select i.e. "<path_to\>MCUX_Provi_v9\bin\_internal\data\sample_data\targets\RW612\source_images\frdmrw612_gpio_led_output.s19". Click on the check box of the Configuration Helper message that appeared and click OK. 4. Set your board in ISP mode; Connect the USB cable to your PC via J10 with the ISP (SW3) button pressed. 5. In the options of the tool please select RW612, UART (select the correct PORTx), Plain, Flex SPI NOR - complete FCB, InField shadow regs, No TrustProvi and PyOCD.   6. Click on Build Image 7. Move to Write Image section and click on Write Image 8. Once the example is flashed, the LED in the board should start to blink 9. Power reset your board and try flashing a MCUXpresso SDK hello_world    I hope this helps. Regards, Daniel.  
View full article
Sometimes, we need to assign a static IP to Wi-Fi chip which is working in STA mode to do test based on Linux platform. In this article, shared the steps to assign a static IP address for 88W8997 which is working in STA mode based on Linux. And you can also refer this method to set static IP for other Wi-Fi chips.
View full article
This article gives detailed hands-on steps about how to do Bluetooth A2DP music playing and Wi-Fi 2.4G iperf throughout coexist test. The hands-on test is based on 88W8997 with I.MX8MQ which is based on Linux 5.15.71 host platform. Using driver is  Q1-2024 released Wi-Fi driver + Q1-2024 released FW version. You can refer to this article to do similar Bluetooth A2DP music playing and Wi-Fi 2.4G iperf throughout test on other Wi-Fi/Bluetooth chips based on other Linux platform. For detailed steps, please refer to attached pdf file.   Best regards, Christine.
View full article
The article introduces steps on how to build RW612 zigbee source code, it includes the following contents: 1. Introduction 2. Preparation before compilation       2.1 CMake       2.2 Ninja       2.3 ARM GCC tool chain      2.4 Python3      2.5 MCUXPress SDK 3. Building Zibgee Source Code on ubuntu 20.04 host      3.1 Setting up environment      3.2 Compilation steps 4. Compilation on other ubuntu host      4.1 ubuntu 22.04      4.2 ubuntu 24.04 5. Verified ARM GCC Version 6. Programing QSPI Nor Flash   NXP TIC connectivity team  Weidong Sun May-15-2025
View full article
In the context of TF-M(Trusted Firmware-M), BL2 refers to the second stage bootloader. When using TF-M, the BL2 is based on open-source MCUBoot. It is responsible for verifying and loading the secure and non-secure images.  Our MCUXpresso SDK takes the open-source MCUBoot and leverages the HW features available to the specific SoC that is being used. In addition, TF-M support for the SoC is also available in the SDK package. Current configuration of TF-M within the SDK does not support enabling BL2. The following steps demonstrate how to configure the TF-M project in the SDK, so that it can be linked directly with MCUBOOT from our SDK without enabling BL2.  Import MCUBOOT_OPENSOURCE example Select Import SDK Example and select the board you are working with. Browse the ota_examples to find the mcuboot_opensource example. Select this and press Next. The following window will contain the memory configuration of the example. It is important to change the Location address(0x18000000) to the secure alias and the Driver(*_S.cfx) to the secure version of the driver. Then press Finish.   Locate the flash_partioning.h header file within the project to determine the start address of where the TF-M secure image will be located. This will be represented by the BOOT_FLASH_ACT_APP macro. #define BOOT_FLASH_ACT_APP 0x18020000. In this example, I know that the secure image should be located in the offset 0x20000. Additionally, using MCUBoot means that we will have a header attached to the image when signed, this will add an addition 0x400. In total my offset will be 0x20400.  Open the preprocessor configurations in the project by right clicking the project and select Properties. With the window open navigate to the following location: C/C++ Build -> Settings -> MCU C Compiler -> Preprocessor Set BOOT_HEADER_ENABLE = 0 Press Apply and Close. Build mcuboot image. Import TFM_DEMO_S/NS example Select Import SDK Example and select the board you are working with. Browse the tfm_examples to find the tfm_demo_s/ns examples. Select these and import.  Open the preprocessor configurations in the project by right clicking the project and select Properties. With the window open navigate to the following location: C/C++ Build -> Settings -> MCU C Compiler -> Preprocessor Set BOOT_HEADER_ENABLE = 0 Open the flash_layout.h header file under the following folder in the tfm_demo_s project: tf-m/platform/ext/target/nxp/*board*/partition/ Edit the FLASH_IMAGE_HEADER_SIZE macro. Since we know that MCUBoot uses a header this will be equal to 0x400. #define FLASH_IMAGE_HEADER_SIZE (0x400) Open the region_defs.h header file under the following folder: tf-m/platform/ext/target/nxp/*board*/partition/ Edit the S_IMAGE_PRIMARY_PARTITION_OFFSET macro. Based on the calculated above, the offset used in this example of the primary image will be 0x20400. #define S_IMAGE_PRIMARY_PARTITION_OFFSET (0x20400) Edit the M_BOOT_FLASH_CONF_START macro. This should be the same as the base address being used in MCUBoot's BOOT_FLASH_ACT_APP. #define M_BOOT_FLASH_CONF_START (0x18020000) Open the startup_*board*.c source file under the following folder: tf-m/platform/ext/target/nxp/*board*/Device/Source Edit the void Reset_Handler(void) function. Add the VTOR configuration so that it points to the top of the vector table.  // Config VTOR & MSPLIM register __asm volatile ("LDR R0, =0xE000ED08 \n" "STR %0, [R0] \n" "LDR R1, [%0] \n" "MSR MSP, R1 \n" "MSR MSPLIM, %1 \n" : : "r"(__VECTOR_TABLE), "r"(__STACK_LIMIT) : "r0", "r1"); *Note: This step is only done on the secure image. Press Apply and Close. Build secure image. Repeat the same steps 2- 8 in this section for the non-secure image and build. Generate Binaries Under the Debug folder you will find the .axf file generated automatically by MCUXpresso IDE under the secure project. Right click on this and navigate to Binary Utilities -> Create Binary.  Repeat for non-secure image. Merge Binaries Note: This article does not show detailed steps of using the SPSDK command line tool. If detailed steps are needed please refer to spsdk.readthedocs.io.  Use the following command to generate the template to merge the binaries. nxpimage utils binary-image get-template -o binary_merge_template.yaml Edit the template. Calculate the offset of the location of the non-secure image using FLASH_S_PARTITION_SIZE from the flash_layout.h header file. In this example the value is 0x9FC00.   Use the following command to merge the binaries. nxpimage utils binary-image merge -c binary_merge_template.yaml -o merged_tfm_demo.bin   Use Secure Provisioning Tool to Sign Images Note: This article does not show detailed steps of using MCUXpresso Secure Provisioning Tool. If detailed steps are needed please refer to the its user guide available in the Help Menu of the tool.  Select the MCUBOOT_OPENSOURCE image as your source. Open the MCUBoot -> Sign Image tool.  Select the merged binary as your source. The output image should be filled automatically to the bootable_images folder of the secure provisioning workspace. Select the key used to authenticate the image. In mcuboot_opensource workspace there is a key folders that contain example keys used for development.   4. Press Sign, then make sure that the target address matches the based address defined in the mcuboot for the primary partition, then save & close.  5. Build and Write Image accordingly with the Secure Provisioning Tool.  Run Application  
View full article
The article introduces steps on how to transmit files between IW612 Bluetooth and remote devices on linux platform.   NXP TIC Connectivity Team Weidong Sun
View full article
The article introduces the following contents related to 88W9098. 1. Introduction     1.1 Software Tools     1.2 Hardware Tools     1.3 Diagram of connections 2. Configurations     2.1 Loading Wi-Fi driver     2.2 Connecting external AP          2.2.1 mlan0 to external AP with 5G          2.2.2 mmlan0 to Mobile with 2.4G 2.3 Configuring iptables 2.4 DHCP service on ethernet 3. Wi-Fi Bridge Verification     3.1 Verification of Ethernet to mlan0     3.2 Verification of Ethernet to mmlan0   NXP TIC Connectivity Team Weidong Sun  
View full article
The article will introduce the following contents. No.1 Preparation          1. Ubuntu 20.04 Host          2. Downloading Mass Market Driver(FP92)source code No.2 For ARM Platform          1. Toolchain For cross compilation          2. Linux Kernel source code of target board          3. Building Linux Kernel source code of target board          4. Building NXP Wi-Fi Mass Market Driver source code No.3 For X86 Platform          1. Compilation on different ubuntu version 1.1 Ubuntu 16.04 LTS 1.2 Ubuntu 18.04 LTS 1.3 Ubuntu 20.04 LTS 1.4 Ubuntu 22.04 LTS         2. Cross Compilation on Ubuntu 20.04 LTS 2.1 Linux kernel 4.9 2.2 Linux kernel 5.10 2.3 Linux kernel 6.12 No.4 Conclusion     NXP TIC Connectivity Team Weidong Sun Apr-18-2025
View full article
The article described steps on how to enable SDIO Wi-Fi & Bluetooth on M.2 interface. The main contents are like below: ========================= 1. Introduction  2. Steps            2.1 Board Configurations            ① BoardConfig.mk            ② evk_8mp.mk            ③ SharedBoardConfig.mk            ④ imx8mp_gki.fragment           2.2 Wi-Fi & Bluetooth Configurations            ① wifi_mod_para.conf            ② bt_vendor.conf            ③ vendor_interface.cc  3. Building & Downloading images to i.MX8MP-EVK          3.1 Building images          3.2 Downloading images  4. Running Android images to verify Wi-Fi & Bluetooth  =========================   For other versions of Android bsp or SDIO Wi-Fi/BT on M.2, same steps.   NXP TIC Connectivity Team, Weidong Sun    
View full article
Hardware board : NXP i.MX8MN-EVK  Wi-Fi module on the board is 88W8987. Software : BSP is i.MX Yocto Linux BSP L6.12.3_1.0.0.   Topic: Wi-Fi driver configuration :  wifi_mod_para.conf file How to load the Wi-Fi driver How to use hostapd to configure the 2G connection (uap0) How to start the uap0 2G connection How to use hostapd to configure the 5G connection (uap0) How to start the uap0 5G connection uap0 + ethernet connection    
View full article
Learn how to bring Wi-Fi connectivity to Zephyr’s projects based on the FRDM-RW612 board. This guide walks you through adapting the Ethernet-based mqtt_publisher sample to work over Wi-Fi using Zephyr v4.2.0. You'll explore the built-in wifi/shell example, configure the networking stack, and create a custom shell command to control MQTT publishing. Perfect for developers building IoT applications that need seamless cloud communication over wireless networks.
View full article
Hardware : i.MX8MN-EVK Wi-Fi module on the board is 88W8987. Software: BSP is i.MX Yocto Linux BSP L6.12.3_1.0.0.   Topics: Introduction of Wi-Fi driver configuration file : wifi_mod_para.conf  How to load the Wi-Fi driver How to configure the WPA2/WPA3  5G/2G connection How to use wpa_supplicant to connect to the AP Introduction of some wpa_supplicant.conf parameters    
View full article
This document summary BT classical RF parameters and give examples of nxp wif&bt product Bluetooth rf test and results analysis. The document includes:  Introduction BT key parameters Test Procedure & Result Analysis
View full article