flashing error : RD-RW61x-BGA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

flashing error : RD-RW61x-BGA

2,865 次查看
jigar-maheshwari
Contributor II

Not able to flash anything on RD-RW61x-BGA, 

While connecting with SWD

Connecting to target via SWD

InitTarget() start

SWD selected. Executing JTAG -> SWD switching sequence.

Error: Failed to initialized DAP.

InitTarget() end - Took 2.41ms

Connect fallback: Reset via Reset pin & Connect.

InitTarget() start

SWD selected. Executing JTAG -> SWD switching sequence.

Error: Failed to initialized DAP.

InitTarget() end - Took 2.40ms

Error occurred: Could not connect to the target device.

For troubleshooting steps visit: https://wiki.segger.com/J-Link_Troubleshooting

J-Link>

 

While connecting with USB

J-Link>connect

Device "RW612" selected.



Connecting to target via SWD

InitTarget() start

SWD selected. Executing JTAG -> SWD switching sequence.

DAP initialized successfully.

  DMAP_REG_ID: DM-AP IDCODE detected: 0xFFFFFFFF

ERROR: Wrong DM-AP IDCODE detected: 0xFFFFFFFF

InitTarget() end - Took 201ms

InitTarget() start

SWD selected. Executing JTAG -> SWD switching sequence.

Error: Failed to initialized DAP.

InitTarget() end - Took 102ms

Error occurred: Could not connect to the target device.

For troubleshooting steps visit: https://wiki.segger.com/J-Link_Troubleshooting

J-Link>

in last i have flashed that base_image project binary.

 

0 项奖励
回复
5 回复数

2,840 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

 

Could you please confirm that you are using the correct SDK ? Could you please confirm the version of the SDK? 

 

Regards

0 项奖励
回复

2,826 次查看
jigar-maheshwari
Contributor II
Yes, I am using the proper SDK, from which I have already tried and tested a few other examples that worked fine. However, after I created a custom example and flashed it, this problem arose. this is the version of the sdk i am using SDK_2.16.100_RD-RW612-BGA.
0 项奖励
回复

2,819 次查看
jigar-maheshwari
Contributor II

The last flashed program is working fine, and I can still see its debug logs. However, I am unable to flash a new program onto it.

0 项奖励
回复

2,716 次查看
sofiaurueta
NXP Employee
NXP Employee

Hello,

 

Could you try doing a mass erase? This can be done with the GUI Flash Tool.

 

You could also try using an external J-Link debugger through J19.

Please make sure RF_CNTL_2 is set to 1 as stated in the schematic.

 

 

Best regards.

0 项奖励
回复

2,857 次查看
jigar-maheshwari
Contributor II
 
0 项奖励
回复