flashing error : RD-RW61x-BGA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flashing error : RD-RW61x-BGA

2,868件の閲覧回数
jigar-maheshwari
Contributor II

Not able to flash anything on RD-RW61x-BGA, 

While connecting with SWD

Connecting to target via SWD

InitTarget() start

SWD selected. Executing JTAG -> SWD switching sequence.

Error: Failed to initialized DAP.

InitTarget() end - Took 2.41ms

Connect fallback: Reset via Reset pin & Connect.

InitTarget() start

SWD selected. Executing JTAG -> SWD switching sequence.

Error: Failed to initialized DAP.

InitTarget() end - Took 2.40ms

Error occurred: Could not connect to the target device.

For troubleshooting steps visit: https://wiki.segger.com/J-Link_Troubleshooting

J-Link>

 

While connecting with USB

J-Link>connect

Device "RW612" selected.



Connecting to target via SWD

InitTarget() start

SWD selected. Executing JTAG -> SWD switching sequence.

DAP initialized successfully.

  DMAP_REG_ID: DM-AP IDCODE detected: 0xFFFFFFFF

ERROR: Wrong DM-AP IDCODE detected: 0xFFFFFFFF

InitTarget() end - Took 201ms

InitTarget() start

SWD selected. Executing JTAG -> SWD switching sequence.

Error: Failed to initialized DAP.

InitTarget() end - Took 102ms

Error occurred: Could not connect to the target device.

For troubleshooting steps visit: https://wiki.segger.com/J-Link_Troubleshooting

J-Link>

in last i have flashed that base_image project binary.

 

0 件の賞賛
返信
5 返答(返信)

2,843件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

 

Could you please confirm that you are using the correct SDK ? Could you please confirm the version of the SDK? 

 

Regards

0 件の賞賛
返信

2,829件の閲覧回数
jigar-maheshwari
Contributor II
Yes, I am using the proper SDK, from which I have already tried and tested a few other examples that worked fine. However, after I created a custom example and flashed it, this problem arose. this is the version of the sdk i am using SDK_2.16.100_RD-RW612-BGA.
0 件の賞賛
返信

2,822件の閲覧回数
jigar-maheshwari
Contributor II

The last flashed program is working fine, and I can still see its debug logs. However, I am unable to flash a new program onto it.

0 件の賞賛
返信

2,719件の閲覧回数
sofiaurueta
NXP Employee
NXP Employee

Hello,

 

Could you try doing a mass erase? This can be done with the GUI Flash Tool.

 

You could also try using an external J-Link debugger through J19.

Please make sure RF_CNTL_2 is set to 1 as stated in the schematic.

 

 

Best regards.

0 件の賞賛
返信

2,860件の閲覧回数
jigar-maheshwari
Contributor II
 
0 件の賞賛
返信