spanning tree propocol (STP) on ethernet switch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

spanning tree propocol (STP) on ethernet switch

Jump to solution
2,568 Views
vitech
Contributor II

Greetings, comrades! Have some questions about ethernet switch in Vybrid processor. I'm implementing spanning tree protocol on it, facing some difficulties such as: 1) How can i know from which external port I receive current bpdu frame? What will happen when I receive the same frame from 2 different external ports in short period of time? Is learning fifo is the only one way to get this info?

2) when I'm reading data from learning fifo slower then ESW writes there, will I loss info from new frames? Will I lose info with port number & mac address from received frames when learning fifo is full?

3) Are there any examples or demos of STP or maybe RSTP available for internal switch? linux, mqx, baremetal or whatever. maybe for others freescale controllers?

Thanks, Vitaly.

Labels (3)
0 Kudos
Reply
1 Solution
2,184 Views
rendy
NXP Employee
NXP Employee

I'm sorry, unfortunately I'm not aware of such an example.

Regards

Rene

View solution in original post

0 Kudos
Reply
4 Replies
2,184 Views
timesyssupport
Senior Contributor II

Hello Vitaly,

We are not aware of any Vybrid specific STP/RSTP demos in Linux; perhaps there is something in MQX or baremetal, but from our stand point, we have nothing to point to. Unfortunately, we do not have a primer for STP/RSTP to pass along; should anything need changed within the Vybrid switch's firmware, I think Freescale may have to address that - if/when you get to that point, as I do not believe the configuration registers are accessible from userspace.

karinavalencia​ - perhaps Freescale has a networking resource that is more appropriate from a getting started stand-point?

Regards,

Timesys Support

2,184 Views
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ can you comment here?

0 Kudos
Reply
2,185 Views
rendy
NXP Employee
NXP Employee

I'm sorry, unfortunately I'm not aware of such an example.

Regards

Rene

0 Kudos
Reply
2,184 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help here?

0 Kudos
Reply