spanning tree propocol (STP) on ethernet switch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

spanning tree propocol (STP) on ethernet switch

跳至解决方案
3,984 次查看
vitech
Contributor II

Greetings, comrades! Have some questions about ethernet switch in Vybrid processor. I'm implementing spanning tree protocol on it, facing some difficulties such as: 1) How can i know from which external port I receive current bpdu frame? What will happen when I receive the same frame from 2 different external ports in short period of time? Is learning fifo is the only one way to get this info?

2) when I'm reading data from learning fifo slower then ESW writes there, will I loss info from new frames? Will I lose info with port number & mac address from received frames when learning fifo is full?

3) Are there any examples or demos of STP or maybe RSTP available for internal switch? linux, mqx, baremetal or whatever. maybe for others freescale controllers?

Thanks, Vitaly.

标签 (3)
0 项奖励
回复
1 解答
3,600 次查看
rendy
NXP Employee
NXP Employee

I'm sorry, unfortunately I'm not aware of such an example.

Regards

Rene

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,600 次查看
timesyssupport
Senior Contributor II

Hello Vitaly,

We are not aware of any Vybrid specific STP/RSTP demos in Linux; perhaps there is something in MQX or baremetal, but from our stand point, we have nothing to point to. Unfortunately, we do not have a primer for STP/RSTP to pass along; should anything need changed within the Vybrid switch's firmware, I think Freescale may have to address that - if/when you get to that point, as I do not believe the configuration registers are accessible from userspace.

karinavalencia​ - perhaps Freescale has a networking resource that is more appropriate from a getting started stand-point?

Regards,

Timesys Support

3,600 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ can you comment here?

0 项奖励
回复
3,601 次查看
rendy
NXP Employee
NXP Employee

I'm sorry, unfortunately I'm not aware of such an example.

Regards

Rene

0 项奖励
回复
3,600 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help here?

0 项奖励
回复