Vybrid RM note recommendation.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid RM note recommendation.

跳至解决方案
3,072 次查看
ioseph_martinez
NXP Employee
NXP Employee

Hello Guys,

Not sure if this is already recorded for some of the next revisions of the RM for Vybrid (looked for them on the review documents) but it would be good to have a note on the RM that specifies Slice 2 is exclusively used when LPDDR2 is used, either a note or in each register which configures Slice 2 register. (this only applies to LPDDR2)

Thanks,

Ioseph

标记 (3)
0 项奖励
回复
1 解答
2,741 次查看
naoumgitnik
Senior Contributor V

Thanks Ioseph,

I added your illustration:

PHY_REG_32_33_Swapped~1.jpg

It looks like each description down to the Address is correct but everything below the addresses should be swapped for the 2 registers.

/Naoum.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,741 次查看
naoumgitnik
Senior Contributor V

Added into shared-review RM copy - both swapped registers and slice 2.

/NG

2,741 次查看
ioseph_martinez
NXP Employee
NXP Employee

Thanks Naoum, sure, let me know.

By the way, customer also found that the bitfields from phy32 and phy 33 are swapped.

(they should be exactly as phy16 and phy17 for slice 1 are defined since phy32 and phy33 are only change is they are for slice 2)

0 项奖励
回复
2,741 次查看
ioseph_martinez
NXP Employee
NXP Employee

let me be more specific.

PHY32, is DQ timing register for slice 2.

But in the table "DDRMC_PHY32 field descriptions" is wrong, it talks about the DQS. so the actual table for PHY32 is the one called "DDRMC_PHY33 field descriptions"

Also, the register with the bitfields (the picture with the fields and numbers from 31 and 0) is swapped.

The action neede is:

Swap:

- Register picture from 32 to 33

- Field descriptions table from 32 to 33

Thanks.

0 项奖励
回复
2,742 次查看
naoumgitnik
Senior Contributor V

Thanks Ioseph,

I added your illustration:

PHY_REG_32_33_Swapped~1.jpg

It looks like each description down to the Address is correct but everything below the addresses should be swapped for the 2 registers.

/Naoum.

0 项奖励
回复
2,741 次查看
naoumgitnik
Senior Contributor V

Thanks Ioseph,

I will try to make this next week, will possibly have follow-up questions... :smileywink:

/Naoum.

0 项奖励
回复