Can I use the regular JTAG interface to debug both the A5 and M4 cores on the Vf6XX pocessor or do I need the trace port?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can I use the regular JTAG interface to debug both the A5 and M4 cores on the Vf6XX pocessor or do I need the trace port?

1,404 次查看
jamesherrera
Contributor II

I need some of the pins associated with the trace port for my design and need to know if I can debug with just the Vybrid standard interface using the 20 pin header.

标签 (4)
0 项奖励
回复
2 回复数

974 次查看
naoumgitnik
Senior Contributor V

Just rephrasing Jiri, "Yes, you can".

/Naoum.

0 项奖励
回复

974 次查看
jiri-b36968
NXP Employee
NXP Employee

Hi James,

for debug both cores the trace port /lines are not needed.

/Jiri

0 项奖励
回复