OVG 0.4.0 Driver vgCreateConstImageFSL width change

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OVG 0.4.0 Driver vgCreateConstImageFSL width change

Jump to solution
4,928 Views
jasonwilliamson
Contributor II

The vgCreateConstImageFSL() extension requires a stride and width parameter when creating the image.  In OVG driver 0.3.0 these values could be different.  For example:

Allowed in 0.3.0:

Format: VG_sRGB_565_

Width: 17 pixels

Stride: 40 bytes

For OVG driver 0.4.0 there's a requirement that the stride and width match.  This forces the same image to be created as follows:

Required in 0.4.0:

Format: VG_sRGB_565_

Width: 20 pixels

Stride: 40 bytes

In driver 0.4.0 this forces the "pad" on the right edge of the image to be visible.  This pad (3 pixels in the example above) was only required to achieve the 64-bit stride alignment requirement.  For a RGB565 image the pad is not transparent.

This is a major problem for us as we create all our images using the vgCreateConstImageFSL() extension.

1 Solution
4,763 Views
ioseph_martinez
NXP Employee
NXP Employee

I also tried on the latest OpenVG 0.5.0 and seems it is solved.

View solution in original post

0 Kudos
Reply
7 Replies
4,763 Views
ioseph_martinez
NXP Employee
NXP Employee

I talked to R&D, it seems we have an issue with vg const images stride. I have tested and stride was not used at all. They sent me some code probably will be able to take a look on Monday to check if it fixes it.

0 Kudos
Reply
4,763 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Hi ioseph_martinez , do you have an update of this case?

0 Kudos
Reply
4,763 Views
ioseph_martinez
NXP Employee
NXP Employee

Well, I did test the patch and didn't work. This has been raised to the R&D team and will be working close with you guys to have the different bugs priorized and worked out.

4,763 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Do you have any progress on this case?

0 Kudos
Reply
4,764 Views
ioseph_martinez
NXP Employee
NXP Employee

I also tried on the latest OpenVG 0.5.0 and seems it is solved.

0 Kudos
Reply
4,763 Views
jimmikola
Contributor I

Verified that 0.5.0 has the desired operation where stride and width can be different values.

0 Kudos
Reply
4,763 Views
fengwei
NXP Employee
NXP Employee

I need the sample to check the issue. My case just works.

0 Kudos
Reply