Vybrid dcu4regs.h CLUT offset is wrong on OpenVG 0.5.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid dcu4regs.h CLUT offset is wrong on OpenVG 0.5.0

Jump to solution
1,204 Views
ioseph_martinez
NXP Employee
NXP Employee

Hello fengwei

I think the DCU offset is wrong. This was found previously by vincent.aubineau

currently is:

#define DCU_CLUT_OFFSET

0x0000500

But should be:

#define DCU_CLUT_OFFSET0x0000200

According to the reference manua rev 4

"The CLUT/Tile RAM is mapped in the DCU4 32K memory space from address 0x2000

to 0x3FFF. This gives 2048 entries, which provides up to eight full CLUTs for 8 bpp

layers."

Can we have this Change Request for the next release 0.6.0 of the drivers?

Thanks,

Ioseph

Tags (4)
0 Kudos
Reply
1 Solution
1,020 Views
fengwei
NXP Employee
NXP Employee

Ioseph,

Sure. Thank you for your kind mention.

Regards,

Feng Wei

View solution in original post

0 Kudos
Reply
1 Reply
1,021 Views
fengwei
NXP Employee
NXP Employee

Ioseph,

Sure. Thank you for your kind mention.

Regards,

Feng Wei

0 Kudos
Reply