Minimum RCON for QuadSPI Boot ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Minimum RCON for QuadSPI Boot ?

跳至解决方案
1,697 次查看
ChrisNielsen
Contributor III

If I always want to boot from QuadSPI, are the following the only RCON pins that need to be driven?:

BMODE[1:0] = 10 (use RCON)

RCON4-7 = BOOT_CFG1[7:4] = 0000 to select QuadSPI

RCON1 = BOOT_CFG1[1] = 0/1 to select which QuadSPI (0 or 1)

Can I ignore and leave floating ALL other RCON pins and be assured that it will reliably boot from the specified QuadSPI?

Thanks, Chris

0 项奖励
回复
1 解答
1,431 次查看
naoumgitnik
Senior Contributor V

Hello Chris,

I guess, since you are simply quoting our Reference Manual, which does not mention any other RCON bits, it is correct that their states are 'Do not care' for the QuadSPI boot.

Sincerely, Naoum Gitnik.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,432 次查看
naoumgitnik
Senior Contributor V

Hello Chris,

I guess, since you are simply quoting our Reference Manual, which does not mention any other RCON bits, it is correct that their states are 'Do not care' for the QuadSPI boot.

Sincerely, Naoum Gitnik.

0 项奖励
回复
1,431 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi,

  It's also important to tie RCON31 to ground. Otherwise the BootROM stays in an infinite loop and will not boot from any boot interface.

-Anthony

0 项奖励
回复