Minimum RCON for QuadSPI Boot ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Minimum RCON for QuadSPI Boot ?

Jump to solution
2,707 Views
ChrisNielsen
Contributor III

If I always want to boot from QuadSPI, are the following the only RCON pins that need to be driven?:

BMODE[1:0] = 10 (use RCON)

RCON4-7 = BOOT_CFG1[7:4] = 0000 to select QuadSPI

RCON1 = BOOT_CFG1[1] = 0/1 to select which QuadSPI (0 or 1)

Can I ignore and leave floating ALL other RCON pins and be assured that it will reliably boot from the specified QuadSPI?

Thanks, Chris

0 Kudos
Reply
1 Solution
2,441 Views
naoumgitnik
Senior Contributor V

Hello Chris,

I guess, since you are simply quoting our Reference Manual, which does not mention any other RCON bits, it is correct that their states are 'Do not care' for the QuadSPI boot.

Sincerely, Naoum Gitnik.

View solution in original post

0 Kudos
Reply
2 Replies
2,442 Views
naoumgitnik
Senior Contributor V

Hello Chris,

I guess, since you are simply quoting our Reference Manual, which does not mention any other RCON bits, it is correct that their states are 'Do not care' for the QuadSPI boot.

Sincerely, Naoum Gitnik.

0 Kudos
Reply
2,441 Views
anthony_huereca
NXP Employee
NXP Employee

Hi,

  It's also important to tie RCON31 to ground. Otherwise the BootROM stays in an infinite loop and will not boot from any boot interface.

-Anthony

0 Kudos
Reply