Minimum RCON for QuadSPI Boot ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Minimum RCON for QuadSPI Boot ?

ソリューションへジャンプ
2,715件の閲覧回数
ChrisNielsen
Contributor III

If I always want to boot from QuadSPI, are the following the only RCON pins that need to be driven?:

BMODE[1:0] = 10 (use RCON)

RCON4-7 = BOOT_CFG1[7:4] = 0000 to select QuadSPI

RCON1 = BOOT_CFG1[1] = 0/1 to select which QuadSPI (0 or 1)

Can I ignore and leave floating ALL other RCON pins and be assured that it will reliably boot from the specified QuadSPI?

Thanks, Chris

0 件の賞賛
返信
1 解決策
2,449件の閲覧回数
naoumgitnik
Senior Contributor V

Hello Chris,

I guess, since you are simply quoting our Reference Manual, which does not mention any other RCON bits, it is correct that their states are 'Do not care' for the QuadSPI boot.

Sincerely, Naoum Gitnik.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,450件の閲覧回数
naoumgitnik
Senior Contributor V

Hello Chris,

I guess, since you are simply quoting our Reference Manual, which does not mention any other RCON bits, it is correct that their states are 'Do not care' for the QuadSPI boot.

Sincerely, Naoum Gitnik.

0 件の賞賛
返信
2,449件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi,

  It's also important to tie RCON31 to ground. Otherwise the BootROM stays in an infinite loop and will not boot from any boot interface.

-Anthony

0 件の賞賛
返信