Maximum NAND flash.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,514件の閲覧回数
gelkov
Contributor I

Hello I am investigating the reference manual for Vybrid processor R-series. I am tiring to find the is there are limitations for the maximum size of the NAND flash connected to the Vybrid. Do you have any recommendations about using 512MB NAND?

0 件の賞賛
返信
1 解決策
5,359件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,360件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
5,359件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Hello Maxim,

NAND flashes use 5 cycle addressing:

pastedImage_0.png

In NFC you can select address by:

column NFC_CAR - 2 bytes

row NFC_RAR - 3 bytes + 2 CS.

So theoretically it is really big memory.

No official recommendation for 512MB. On TWR-VF65 we use MT29F2G16ABAEAWP:E 256MB (2Gb).

/Jiri