Maximum NAND flash.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum NAND flash.

Jump to solution
5,573 Views
gelkov
Contributor I

Hello I am investigating the reference manual for Vybrid processor R-series. I am tiring to find the is there are limitations for the maximum size of the NAND flash connected to the Vybrid. Do you have any recommendations about using 512MB NAND?

0 Kudos
Reply
1 Solution
5,418 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
5,419 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
5,418 Views
jiri-b36968
NXP Employee
NXP Employee

Hello Maxim,

NAND flashes use 5 cycle addressing:

pastedImage_0.png

In NFC you can select address by:

column NFC_CAR - 2 bytes

row NFC_RAR - 3 bytes + 2 CS.

So theoretically it is really big memory.

No official recommendation for 512MB. On TWR-VF65 we use MT29F2G16ABAEAWP:E 256MB (2Gb).

/Jiri