IOMUX Controller Driver for Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IOMUX Controller Driver for Linux

Jump to solution
2,265 Views
juandiaz
Contributor II

Hello,

I am just tweaking on the Vybrid VF6 SOM from EmCraft and I would like to know if there is software means to handle the IOMUX controller to control I/O multifunction pins on runtime in the Vybrid VF6xx platform.

Labels (2)
0 Kudos
Reply
1 Solution
1,786 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I lack of the Emcraft BSP and its documentation. I recommend you to reach them and ask them directly in their webpage.

Vybrid VF6 SOM Resource Directory

If the kernel is a version greater than 3.10.x I assume that the pinctrl driver must be fatured in their kernel versions.

Best Regards,

Alejandro

View solution in original post

1 Reply
1,787 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I lack of the Emcraft BSP and its documentation. I recommend you to reach them and ask them directly in their webpage.

Vybrid VF6 SOM Resource Directory

If the kernel is a version greater than 3.10.x I assume that the pinctrl driver must be fatured in their kernel versions.

Best Regards,

Alejandro