IOMUX Controller Driver for Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IOMUX Controller Driver for Linux

ソリューションへジャンプ
2,263件の閲覧回数
juandiaz
Contributor II

Hello,

I am just tweaking on the Vybrid VF6 SOM from EmCraft and I would like to know if there is software means to handle the IOMUX controller to control I/O multifunction pins on runtime in the Vybrid VF6xx platform.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,784件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I lack of the Emcraft BSP and its documentation. I recommend you to reach them and ask them directly in their webpage.

Vybrid VF6 SOM Resource Directory

If the kernel is a version greater than 3.10.x I assume that the pinctrl driver must be fatured in their kernel versions.

Best Regards,

Alejandro

元の投稿で解決策を見る

1 返信
1,785件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I lack of the Emcraft BSP and its documentation. I recommend you to reach them and ask them directly in their webpage.

Vybrid VF6 SOM Resource Directory

If the kernel is a version greater than 3.10.x I assume that the pinctrl driver must be fatured in their kernel versions.

Best Regards,

Alejandro