How to set up the Low Power Timer LPTMR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set up the Low Power Timer LPTMR

ソリューションへジャンプ
3,864件の閲覧回数
bennojung
Contributor I

Hello

Im trying to set up the LPTMR module since days, but it doesnt work.

I set it up by processor expert. But it seems is not that easy...

I've done the following:

- Enabled the LPTMR clock in the CPU module (CCM_CCRG2 -> CG0[1:0)

- Set up the LPTMR module:

pastedImage_0.png

When i start debugging, the counter value of the LPTMR is always 0. What is wrong?

I set the clock 'FIRC' to the clock output pin CK01, the clock runs. So i think the LPTMR_CNR should be upcounting?

I read also the counter value in the software, but there it is also always 0.

Do I have to enable something else?

thanks in advice!

ラベル(6)
0 件の賞賛
返信
1 解決策
3,004件の閲覧回数
cyborgnegotiato
Senior Contributor II

Please use newest version which is 10.4.

Thanks,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,004件の閲覧回数
cyborgnegotiato
Senior Contributor II

Hi,

Which version of PE do you use?

Thanks,

Jozef

0 件の賞賛
返信
3,004件の閲覧回数
bennojung
Contributor I

Hello

We use PE Version 10.3.0.

Thanks

0 件の賞賛
返信
3,005件の閲覧回数
cyborgnegotiato
Senior Contributor II

Please use newest version which is 10.4.

Thanks,

Jozef

0 件の賞賛
返信