How to set up the Low Power Timer LPTMR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to set up the Low Power Timer LPTMR

跳至解决方案
2,708 次查看
bennojung
Contributor I

Hello

Im trying to set up the LPTMR module since days, but it doesnt work.

I set it up by processor expert. But it seems is not that easy...

I've done the following:

- Enabled the LPTMR clock in the CPU module (CCM_CCRG2 -> CG0[1:0)

- Set up the LPTMR module:

pastedImage_0.png

When i start debugging, the counter value of the LPTMR is always 0. What is wrong?

I set the clock 'FIRC' to the clock output pin CK01, the clock runs. So i think the LPTMR_CNR should be upcounting?

I read also the counter value in the software, but there it is also always 0.

Do I have to enable something else?

thanks in advice!

标签 (6)
0 项奖励
回复
1 解答
1,848 次查看
cyborgnegotiato
Senior Contributor II

Please use newest version which is 10.4.

Thanks,

Jozef

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,848 次查看
cyborgnegotiato
Senior Contributor II

Hi,

Which version of PE do you use?

Thanks,

Jozef

0 项奖励
回复
1,848 次查看
bennojung
Contributor I

Hello

We use PE Version 10.3.0.

Thanks

0 项奖励
回复
1,849 次查看
cyborgnegotiato
Senior Contributor II

Please use newest version which is 10.4.

Thanks,

Jozef

0 项奖励
回复