The systick interrupt can NOT be mask on vf610 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The systick interrupt can NOT be mask on vf610 board

ソリューションへジャンプ
1,846件の閲覧回数
pingchuanma
Contributor I

Hi experts,

The systick interrupt can NOT be mask on vf610 board.

1. Set the priority for systick to 0xe0.

2. Set the basepri register to 0x10

3. The systick interrupt can still be generated.

The issue can NOT reproduce on K70 board.  Is this a known issue?  Is there any workaroud? Thanks.

Thanks,

Pingchuan

ラベル(3)
0 件の賞賛
返信
1 解決策
1,579件の閲覧回数
cyborgnegotiato
Senior Contributor II

Hi Pingchuan,

Please, double check your code, this is basic functionality of core (Cortex M4), that works.

Thanks,

Jozef.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,580件の閲覧回数
cyborgnegotiato
Senior Contributor II

Hi Pingchuan,

Please, double check your code, this is basic functionality of core (Cortex M4), that works.

Thanks,

Jozef.

0 件の賞賛
返信