question about mpc5606b external power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

question about mpc5606b external power

2,800 Views
jeonghwanchoi
Contributor II

hello

As I know, there are three ways that asserting external power to the mpc5606b.

J1 System Power

1-2 External Power 9 V DC to 12 V DC Regulated Down to 5 V DC

3-4 USB OSBDM Supplies 5 V DC

5-6 SBC33905 Supplies 5 V DC

I have a 7.2V battery. and I want to assert the power to the mpc5606b board directly.

Is it possible??

0 Kudos
Reply
1 Reply

2,353 Views
FlavioStiffan
NXP Employee
NXP Employee

johnmc(test)​ any clues about this one?

0 Kudos
Reply