question about mpc5606b external power

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

question about mpc5606b external power

2,178 次查看
jeonghwanchoi
Contributor II

hello

As I know, there are three ways that asserting external power to the mpc5606b.

J1 System Power

1-2 External Power 9 V DC to 12 V DC Regulated Down to 5 V DC

3-4 USB OSBDM Supplies 5 V DC

5-6 SBC33905 Supplies 5 V DC

I have a 7.2V battery. and I want to assert the power to the mpc5606b board directly.

Is it possible??

0 项奖励
回复
1 回复

1,731 次查看
FlavioStiffan
NXP Employee
NXP Employee

johnmc(test)​ any clues about this one?

0 项奖励
回复