RSTLED is on

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RSTLED is on

跳至解决方案
6,959 次查看
fahmirazak
Contributor II

hi guys..

want to ask..why my trkmpc560xb when connected to power supply, the RSTLED is on..it is broken or something..?

tq

1 解答
6,472 次查看
DamarisOchoa
NXP Employee
NXP Employee

Hello fahmirazak

I hope  your issue got solved back in may. But if it didn´t, I asked around and the Reset Led is on when you press the reset button, normally. But in case you are not pressing the button, it means the micro is resetting itself. This could mean that there is a program doing it or that there is nothing on the flash. It could also be a problem with the microcontroller.

Depending if you can program you mcu, is if it is broken.

Regards,

在原帖中查看解决方案

0 项奖励
回复
6 回复数
6,473 次查看
DamarisOchoa
NXP Employee
NXP Employee

Hello fahmirazak

I hope  your issue got solved back in may. But if it didn´t, I asked around and the Reset Led is on when you press the reset button, normally. But in case you are not pressing the button, it means the micro is resetting itself. This could mean that there is a program doing it or that there is nothing on the flash. It could also be a problem with the microcontroller.

Depending if you can program you mcu, is if it is broken.

Regards,

0 项奖励
回复
6,472 次查看
rogercovarrubia
Contributor III

The same thing happens to me but once i flash it the led goes off, then when i plug it again to a source power tsomethimes the led goes on again, But it just happens on some programs that i flash i think (I hope) that it is a register that is corrupted or something

0 项奖励
回复
6,472 次查看
rogercovarrubia
Contributor III

Mine is a mpc5606b

0 项奖励
回复
6,472 次查看
FlavioStiffan
NXP Employee
NXP Employee

Can you flash it?

0 项奖励
回复
6,472 次查看
FlavioStiffan
NXP Employee
NXP Employee

murraystewart-b04629 do you have 2 min to check this out? maybe you have an answer to this.

Thanks

6,472 次查看
fahmirazak
Contributor II

cant flash..do you have any idea?

0 项奖励
回复